Questions regarding LX2080A support in LSDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Questions regarding LX2080A support in LSDK

780 Views
sanghun
Contributor I

Hi, I'm Sanghun

 

I have two questions about the LX2080A

 

1.Can LSDK 20.04-update-290520 support LX2080A? And from what version of LSDK is LX2080A supported?


2. In flex-builder, LX2080A is not in the machine list. Can I use LX2160A? Do I need an additional patch when using it?

 

Thank you.

0 Kudos
Reply
3 Replies

769 Views
yipingwang
NXP TechSupport
NXP TechSupport

1. LSDK 20.04-update-290520 supports LX2080A(lx2160), it is supported from LSDK1812 release.

2. You could use LX2160A in LSDK, no need additional patch.

764 Views
sanghun
Contributor I

Thank you for answer.

 

I have one more question.

 

In flex-builder's machine list, there are lx2160ardb and lx2160ardb_rev2.

 

What does the lx2080a use?

 

Thank you.

0 Kudos
Reply

758 Views
yipingwang
NXP TechSupport
NXP TechSupport

Switch Setting for Lx2080 on LX2160ARDB

rev1: SW3[1:3]=10x
rev2: SW3[1:3]=110

The user could use lx2160ardb images according to the target board(rev1 or rev2).

0 Kudos
Reply