Hi,
I am trying to to find the proper processor for my embedded design.
What I need is a processor that supports 10 Gbps Ethernet and at least 8 GB of RAM.
I realize that QorIQ LS1046A has all that I need.
However, for the 10G connection, it says it is compatible with 10GBase-KR.
Thanks,
Solved! Go to Solution.
LS1046A on-chip SerDes can work as a 10GBase-KR or 1000Base-KX PHY, only passive circuitry is necessary to completethe interface. For whatever else, you need an external PHY which: (a) supports the PHY spec you are interested in;
(b) supports one of LS1046A MAC/PHY interfaces: SGMII, SGMII 2.5G, XFI.
Have a great day,
Platon
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
LS1046A on-chip SerDes can work as a 10GBase-KR or 1000Base-KX PHY, only passive circuitry is necessary to completethe interface. For whatever else, you need an external PHY which: (a) supports the PHY spec you are interested in;
(b) supports one of LS1046A MAC/PHY interfaces: SGMII, SGMII 2.5G, XFI.
Have a great day,
Platon
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------