QorIQ LS1021A Reference Manual - QuadSPI - In the QuadSPI_FR field descriptiion (p. 2161) Field 23 ILLINE - missing Refer to Table 1 for a list of legal instructions. Is there existing another document for the QuadSPI which includs all the Refer to Tabl

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QorIQ LS1021A Reference Manual - QuadSPI - In the QuadSPI_FR field descriptiion (p. 2161) Field 23 ILLINE - missing Refer to Table 1 for a list of legal instructions. Is there existing another document for the QuadSPI which includs all the Refer to Tabl

Jump to solution
1,099 Views
rolandeggli
Contributor I

The QuadSPI documentation are not complet

-Chapter 28.4.2.12 Serial Flash Address Register (QuadSPI_SFAR) is referenced to a none existing Table 1

-Chapter 28.4.2.17 TX Buffer Data Register (QuadSPI_TBDR) is referenced to a none existing Table 1

-Chapter 28.4.2.19 Flag Register (QuadSPI_FR ) is referenced to a none existing Table 1

-Chapter 28.4.2.27 RX Buffer Data Register (QuadSPI_RBDRn) is referenced to a none existing Table 1

Do you have another complete documentations which includes the referenced tables.

Specially the section of "list of legal instructions" and "table for the related commands" are the point of interrest

Sincerely Roland

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
963 Views
ufedor
NXP Employee
NXP Employee

> -Chapter 28.4.2.12 Serial Flash Address Register (QuadSPI_SFAR) is referenced to a none existing Table 1

Correction - Table 28-10. Serial Flash Address Assignment

> -Chapter 28.4.2.17 TX Buffer Data Register (QuadSPI_TBDR) is referenced to a none existing Table 1

Correction - Table 28-19. Byte Ordering in Individual Flash Mode

> -Chapter 28.4.2.19 Flag Register (QuadSPI_FR ) is referenced to a none existing Table 1

Correction - Table 28-17. Instruction set

> -Chapter 28.4.2.27 RX Buffer Data Register (QuadSPI_RBDRn) is referenced to a none existing Table 1

Correction - Table 28-19. Byte Ordering in Individual Flash Mode

The typos will be fixed in the next RM revision.

View solution in original post

0 Kudos
Reply
1 Reply
964 Views
ufedor
NXP Employee
NXP Employee

> -Chapter 28.4.2.12 Serial Flash Address Register (QuadSPI_SFAR) is referenced to a none existing Table 1

Correction - Table 28-10. Serial Flash Address Assignment

> -Chapter 28.4.2.17 TX Buffer Data Register (QuadSPI_TBDR) is referenced to a none existing Table 1

Correction - Table 28-19. Byte Ordering in Individual Flash Mode

> -Chapter 28.4.2.19 Flag Register (QuadSPI_FR ) is referenced to a none existing Table 1

Correction - Table 28-17. Instruction set

> -Chapter 28.4.2.27 RX Buffer Data Register (QuadSPI_RBDRn) is referenced to a none existing Table 1

Correction - Table 28-19. Byte Ordering in Individual Flash Mode

The typos will be fixed in the next RM revision.

0 Kudos
Reply