PPS signal based on PTP Hardware Clock for LS1028A-RDB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PPS signal based on PTP Hardware Clock for LS1028A-RDB

跳至解决方案
1,121 次查看
ceroone
Contributor II

Hello,

According to this post (https://community.nxp.com/t5/Other-NXP-Products/PPS-signal-on-LS1021A-TSN/m-p/1296948#M11360), it is possible to generate a PPS signal from the PTP Hardware Clock on the LS1028A-RDB.

Could you please provide me with a link that explains the steps to follow to do this, or at least some additional information?

What about the IMX8MPEVK? Is the PPS signal generation supported on this board too? Is the procedure similar?

Thank you in advance.

ceroone

0 项奖励
回复
1 解答
1,115 次查看
r8070z
NXP Employee
NXP Employee

There is a link to the OpenIL user manual in the post you mentioned, which says the LS1028A-RDB supports the PPS signal, but does not say the same for the IMX8MPEVK. It also provides commands to use and test PPS generation under OpenIL. The corresponding commands in case of using the Layerscape Software Development Kit on LS1028A can be found in the LSDK user manual.
 https://docs.nxp.com/bundle/GUID-3FFCCD77-5220-414D-8664-09E6FB1B02C6/page/GUID-F53B3CE9-AB67-4713-9...
https://docs.nxp.com/bundle/GUID-3FFCCD77-5220-414D-8664-09E6FB1B02C6/page/GUID-F53B3CE9-AB67-4713-9...
The low-level programming model of the LS1028A IEEE 1588 module can be found in Section 16.3 Ethernet Controller (ENETC) of the QorIQ LS1028A Reference Manual. You can download it from the LS1028A web page
https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/layerscape-processors/la...

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,116 次查看
r8070z
NXP Employee
NXP Employee

There is a link to the OpenIL user manual in the post you mentioned, which says the LS1028A-RDB supports the PPS signal, but does not say the same for the IMX8MPEVK. It also provides commands to use and test PPS generation under OpenIL. The corresponding commands in case of using the Layerscape Software Development Kit on LS1028A can be found in the LSDK user manual.
 https://docs.nxp.com/bundle/GUID-3FFCCD77-5220-414D-8664-09E6FB1B02C6/page/GUID-F53B3CE9-AB67-4713-9...
https://docs.nxp.com/bundle/GUID-3FFCCD77-5220-414D-8664-09E6FB1B02C6/page/GUID-F53B3CE9-AB67-4713-9...
The low-level programming model of the LS1028A IEEE 1588 module can be found in Section 16.3 Ethernet Controller (ENETC) of the QorIQ LS1028A Reference Manual. You can download it from the LS1028A web page
https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/layerscape-processors/la...

0 项奖励
回复