PME software in QorIQ SDK v2.0-1703

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PME software in QorIQ SDK v2.0-1703

935 Views
nic30
Contributor I

Hello,

which yocto packages are required to run PME on LS2088ardb?

I am using QorIQ SDK v2.0-1703.

I see that fsl-pme package does not support LS2088 and simple adding LS2088 to compatibility list does not work.

Also in original firmware shipped with this board there is not any tool starting with pme*.

root@ls2088ardb:~# dmesg | grep -i "PME"
[    1.782652] pci 0000:00:00.0: PME# supported from D0 D1 D2 D3hot
[    1.783583] pci 0000:01:00.0: PME# supported from D0 D3hot D3cold
[    1.889412] pcieport 0000:00:00.0: Signaling PME through PCIe PME interrupt
[    1.896415] pci 0000:01:00.0: Signaling PME through PCIe PME interrupt
[    1.902981] pcie_pme 0000:00:00.0:pcie01: service driver pcie_pme loaded
[    1.903059] layerscape-pcie 3600000.pcie: failed to get PME IRQ: -6
[    1.909357] layerscape-pcie 3600000.pcie: failed to initialize PME
[    1.963337] pci 0001:00:00.0: PME# supported from D0 D1 D2 D3hot
[    1.984208] pcieport 0001:00:00.0: Signaling PME through PCIe PME interrupt
[    1.991212] pcie_pme 0001:00:00.0:pcie01: service driver pcie_pme loaded
[    1.991279] layerscape-pcie 3700000.pcie: failed to get PME IRQ: -6
[    1.997576] layerscape-pcie 3700000.pcie: failed to initialize PME

Is PME supported in this processor?

Labels (1)
0 Kudos
Reply
1 Reply

637 Views
yipingwang
NXP TechSupport
NXP TechSupport

So far no PME enablement SW is done on DPAA2 devices yet.

We have not scheduled any enablement work for PME on the LS2 series of products.It currently is not planned for any SDK release.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply