No output from UBOOT serial port

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

No output from UBOOT serial port

跳至解决方案
1,022 次查看
muaxi8
Contributor V

My uboot code has already loaded into the DDR. I used codewarrior to step through the init_sequence_f sequence, but there is no output from the serial port. Is there anything I need to set?What could be the problem.

muaxi8_0-1626849572545.png

 

0 项奖励
回复
1 解答
1,017 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please click "Debug" to connect CodeWarrior to the target board, the debugger stops at _start symbol first. Click "Resume" button to let u-boot continue running, then click "Suspend" button to check where u-boot is stuck.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,018 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please click "Debug" to connect CodeWarrior to the target board, the debugger stops at _start symbol first. Click "Resume" button to let u-boot continue running, then click "Suspend" button to check where u-boot is stuck.

0 项奖励
回复
996 次查看
muaxi8
Contributor V

erratum_a050106();this function can not Performed in the past, After it is removed,uboot can bring up

0 项奖励
回复
1,012 次查看
muaxi8
Contributor V

 

1:click "Debug" to connect CodeWarrior to the target board, the debugger stops at _start symbol :

muaxi8_0-1626861551594.png

2:Click "Resume" button to let u-boot continue running, The suspend button is grayed out and cannot be used

muaxi8_1-1626861596147.png

 

3: Continue to click the Resum button and Resume grays out, No call stack

muaxi8_2-1626861615354.png

 

 

 

0 项奖励
回复