Mini PCIe not detected on LS1043ARDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mini PCIe not detected on LS1043ARDB

1,829 Views
mehdi-cubic
Contributor II

I have been unable to resolve the issue I posted here. Trying to use Sierra Modem EM9191 (also Telit FN990A) on LS1043ARDB.

Using M.2 to Mini PCIe adapter board (Techship MP301-ES) and u-boot does not detect the device on the PCI bus (see console output below).

I can successfully detect and run WiFi module 920NGW on this PCI bus (of course with different adapter board)

Please let me know if this is expected to work with the default configuration of nxp-qoriq build or if there are any changes that I can try on the configuration (e.g. RCW).

----------------

Using SERDES1 Protocol: 5205 (0x1455)
PCIe1: pcie@3400000 disabled
PCIe2: pcie@3500000 Root Complex: no link
PCIe3: pcie@3600000 Root Complex: no link

------------------

Thank you.

0 Kudos
Reply
4 Replies

1,744 Views
yipingwang
NXP TechSupport
NXP TechSupport

Can you check and tell us the PCIe LTSSM state[from PCI Express Link Control Register] at Uboot when you are connecting the Telit FN990A via M.2 to Mini PCIe adapter board ?

0 Kudos
Reply

1,739 Views
mehdi-cubic
Contributor II

Hello,
Thanks for the update. 
Yes sure, I will extract the value in this register and post it ASAP.

0 Kudos
Reply

1,796 Views
yipingwang
NXP TechSupport
NXP TechSupport

Discussing with the AE team.

0 Kudos
Reply

1,757 Views
mehdi-cubic
Contributor II

I assume there has been no progress on this topic?

0 Kudos
Reply