M.2 SSD in LS1046 custom board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

M.2 SSD in LS1046 custom board

ソリューションへジャンプ
629件の閲覧回数
Ellu24
Contributor III

I am designing a hardware using LS1046. In our design, we are planning to use M.2 SSD PCIe3.0x4 instead of eMMC or SDcard. We are planning to connect M.2 SSD using USB -PCIe bridge. My questions are:

1) Can I use M.2 SSD instead of eMMC or SDcard and will the processor support the same?

2) Is it compatible for the processor to use the USB -PCIe bridge?

 

Thanking you in advance

 

タグ(1)
0 件の賞賛
返信
1 解決策
594件の閲覧回数
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @Ellu24,

LS1046A can boot from SD/eMMC. It cannot boot from SSD. So if you use SSD, you need to use some other boot source.

You are planning to use USB-PCIe bridge. I'm not sure why you do not plan to connect M.2 SSD directly to PCIe controller of LS1046A. This will give you very high throughput.

The USB controller of LS1046A complies with USB specification rev 3.0. You can plug-in anything that complies to the specification.

Regards,
Mrudang

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
595件の閲覧回数
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @Ellu24,

LS1046A can boot from SD/eMMC. It cannot boot from SSD. So if you use SSD, you need to use some other boot source.

You are planning to use USB-PCIe bridge. I'm not sure why you do not plan to connect M.2 SSD directly to PCIe controller of LS1046A. This will give you very high throughput.

The USB controller of LS1046A complies with USB specification rev 3.0. You can plug-in anything that complies to the specification.

Regards,
Mrudang

0 件の賞賛
返信
584件の閲覧回数
Ellu24
Contributor III

Thank you very much for your reply.

0 件の賞賛
返信