Hi, I meet a problem: I desigend a board with ls1046(1.2GHz), reffer to ls1046rdb. A simple boot which print i++, runs and abnormally crash with no time regularity, maybe crash in a few seconds or in a few minutes or one hour.
I have measured the power supply & clk , nothing abnormal found.
I found that, the signal "hreset" may drop down a short time, "hreset" I use as input signal,4.7K res pull up, that means I do not drive on the signal . I also found "ifc_clk" change from 50MHz to 12.5MHz, when Ls1046 crash., If not crash ,it will be always 50MHz. So, it seems LS1046'PLL crash.
One mistake is that, I used 1.0v to power the vdd, when I check the datasheet, it should be 0.9v(1.2Ghz), will this destroy the IC? I have correct the vdd to 0.9v, but I cannot find anything abnormal in these days. may somebody help me ?
Thanks a lot.
解決済! 解決策の投稿を見る。
Problem is solved.
First, 1.0V vdd will not damage ls1046 of 1.2GHz version.
Second, on my board, the "poreset_B" signal is interfered by the board main power, which is DC_12V. I found that, the higher Voltage of power(like 13V), more possibly LS1046 crash. And when I measured the "poreset_B" signal , Ls1046 can run well.
So, I suggest "poreset_B" have aresistance pullup and 22pF cap to ground, that will be beneficial.
I have thinking about why "poreset_b" be interfaced these days, And found the vdd power ltc3866 may have some problem . I designed the ltc3866 reffer to the demo, but much high overshoot (p2p 22v max)found on the "sw" pin, that will worsen the board power supply dc-12v, and the the dc-12v interfaces the "poreset_b".
I check the datasheet of ltc3866, and want to ask why "sgnd"&"gnd" are not one net, but connect them by 0Ω-res(on the bom ,there is no this 0Ω unexpectedly )? Dose anybody have the same problem?
Thanks.
Problem is solved.
First, 1.0V vdd will not damage ls1046 of 1.2GHz version.
Second, on my board, the "poreset_B" signal is interfered by the board main power, which is DC_12V. I found that, the higher Voltage of power(like 13V), more possibly LS1046 crash. And when I measured the "poreset_B" signal , Ls1046 can run well.
So, I suggest "poreset_B" have aresistance pullup and 22pF cap to ground, that will be beneficial.