I am trying to bring up an LX2160A-RDB-B that I just received (presuming that means rev2). I set up a Ubuntu 22.04 VM, installed the tools and used bitbake to make these images: boot_lx2160ardb-rev2_lts_6.1.tgz, ls-image-main-lx2160ardb-rev2.tar.gz, and lx2160ardb-rev2/firmware_lx2160ardb-rev2_uboot_sdboot.img in the build_lx2160ardb-rev2/tmp/deploy/images/ directory. I then used tinyLinux and flex_installer to format and download the images to both a SATA HD and when that didn't work, the supplied SD Card.
flex-installer -i pf -d /dev/sda
flex-installer -b boot_lx2160ardb-rev2_lts_6.1.tgz -r ls-image-main-lx2160ardb-rev2.tar.gz -f firmware_lx2160ardb-rev2_uboot_sdboot.img -d /dev/sda
flex-installer -i pf -d /dev/mmcblk0
flex-installer -b boot_lx2160ardb-rev2_lts_6.1.tgz -r ls-image-main-lx2160ardb-rev2.tar.gz -f firmware_lx2160ardb-rev2_uboot_sdboot.img -d /dev/mmcblk0
Neither image boots, the relevant console output is
Device 0: unknown device
switch to partitions #0, OK
mmc0 is current device
Scanning mmc 0:1…
Scanning mmc 0:2…
Found U-Boot script /lx2160ardb_boot.scr
980 bytes read in 12 ms (79.1 KiB/s)
## Executing script at 80000000
Bad Linux ARM64 Image magic!
SCRIPT FAILED: continuing…
Scanning mmc 0:3…
Scanning mmc 0:4…
switch to partitions #0, OK
mmc1(part 0) is current device
** No partition table - mmc 1 **
scanning bus for devices…
Target spinup took 0 ms.
AHCI 0001.0301 32 slots 1 ports 6 Gbps 0x1 impl SATA mode
flags: 64bit ncq pm clo only pmp fbss pio slum part ccc apst
Device 0: (0:0) Vendor: ATA Prod.: Samsung SSD 870 Rev: SVT0
Type: Hard Disk
Capacity: 476940.0 MB = 465.7 GB (976773168 x 512)
SATA link 0 timeout.
AHCI 0001.0301 32 slots 1 ports 6 Gbps 0x1 impl SATA mode
flags: 64bit ncq pm clo only pmp fbss pio slum part ccc apst
SATA link 0 timeout.
AHCI 0001.0301 32 slots 1 ports 6 Gbps 0x1 impl SATA mode
flags: 64bit ncq pm clo only pmp fbss pio slum part ccc apst
SATA link 0 timeout.
AHCI 0001.0301 32 slots 1 ports 6 Gbps 0x1 impl SATA mode
flags: 64bit ncq pm clo only pmp fbss pio slum part ccc apst
Device 0: (0:0) Vendor: ATA Prod.: Samsung SSD 870 Rev: SVT0
Type: Hard Disk
Capacity: 476940.0 MB = 465.7 GB (976773168 x 512)
… is now current device
Scanning scsi 0:1…
Scanning scsi 0:2…
Found U-Boot script /lx2160ardb_boot.scr
980 bytes read in 5 ms (191.4 KiB/s)
## Executing script at 80000000
Bad Linux ARM64 Image magic!
SCRIPT FAILED: continuing…
解決済! 解決策の投稿を見る。
Please make sure that you are using the correct flex-installer script.
$ git clone https://github.com/nxp-imx/meta-nxp-desktop.git -b
lf-6.1.36-2.1.0-mickledore
$ cp meta-nxp-desktop/scripts/flex-installer_1.14.2110.lf /usr/bin/flexinstaller
$ sudo chmod a+x /usr/bin/flex-installer
$ which flex-installer
Please make sure that you are using the correct flex-installer script.
$ git clone https://github.com/nxp-imx/meta-nxp-desktop.git -b
lf-6.1.36-2.1.0-mickledore
$ cp meta-nxp-desktop/scripts/flex-installer_1.14.2110.lf /usr/bin/flexinstaller
$ sudo chmod a+x /usr/bin/flex-installer
$ which flex-installer
I was running on the tinyLinux from the on-board flash and could not easily run flex-installer on the host. I copied the latest flex-installer and the previously build images to the tinyLinux ramdisk in the root home directory and ran flex-installer from there. Both the SD-card and SATA disk are booting.
The SATA partitions contain these files:
root@TinyLinux:~# ls -l /mnt/*
/mnt/sda1:
total 16
drwx——— 2 root root 16384 Aug 23 17:15 lost+found
/mnt/sda2:
total 59712
-rw-r———r——— 1 1000 1000 45070848 Dec 12 2023 Image
-rw-r———r——— 1 1000 1000 15898458 Dec 12 2023 Image.gz
-rw-r———r——— 1 1000 1000 33525 Dec 12 2023 fsl-lx2160a-qds-lx2160ardb-rev2.dtb
-rw-r———r——— 1 1000 1000 33525 Dec 12 2023 fsl-lx2160a-qds.dtb
-rw-r———r——— 1 1000 1000 34234 Dec 12 2023 fsl-lx2160a-rdb-lx2160ardb-rev2.dtb
-rw-r———r——— 1 1000 1000 34234 Dec 12 2023 fsl-lx2160a-rdb.dtb
drwx——— 2 root root 16384 Aug 23 17:15 lost+found
-rw-r———r——— 1 1000 1000 980 Dec 12 2023 lx2160ardb_boot.scr
drwxr-xr-x 3 1000 1000 4096 Sep 4 2023 modules
/mnt/sda3:
total 16
drwx——— 2 root root 16384 Aug 23 17:16 lost+found
/mnt/sda4:
total 878956
lrwxrwxrwx 1 root root 7 Aug 27 18:37 bin -> usr/bin
drwxr-xr-x 2 root root 4096 Aug 27 18:37 boot
-rw-r———r——— 1 root root 79345412 Aug 27 16:50 boot_lx2160ardb-rev2_lts_6.1.tgz
drwxr-xr-x 2 root root 4096 Mar 9 2018 dev
drwxr-xr-x 97 root root 4096 Aug 27 18:37 etc
-rw-r———r——— 1 root root 57551852 Aug 27 18:18 firmware_lx2160ardb-rev2_uboot_sdboot.img
drwxr-xr-x 3 root root 4096 Aug 27 18:37 home
lrwxrwxrwx 1 root root 7 Aug 27 18:37 lib -> usr/lib
drwx——— 2 root root 16384 Aug 23 17:16 lost+found
-rw-r———r——— 1 root root 763064905 Aug 27 16:49 ls-image-main-lx2160ardb-rev2.tar.gz
drwxr-xr-x 2 root root 4096 Mar 9 2018 media
drwxr-xr-x 2 root root 4096 Mar 9 2018 mnt
drwxr-xr-x 2 root root 4096 Mar 9 2018 opt
drwxr-xr-x 2 root root 4096 Mar 9 2018 proc
drwx——— 2 root root 4096 Aug 27 18:37 root
drwxr-xr-x 7 root root 4096 Aug 27 18:37 run
lrwxrwxrwx 1 root root 8 Aug 27 18:37 sbin -> usr/sbin
drwxr-xr-x 2 root root 4096 Mar 9 2018 srv
drwxr-xr-x 2 root root 4096 Mar 9 2018 sys
drwxrwxrwt 4 root root 4096 Aug 27 18:37 tmp
drwxr-xr-x 12 root root 4096 Aug 27 18:37 usr
drwxr-xr-x 12 root root 4096 Aug 27 18:37 var
root@TinyLinux:/mnt/sda2# cat /mnt/sda2/lx2160ardb_boot.scr
‘VN aM›ð”
ôŒ
env exists dtb || setenv dtb fsl-lx2160a-rdb.dtb;env exists kernel_image || setenv kernel_image Image;env exists devpart_boot || setenv devpart_boot 1;env exists devpart_root || setenv devpart_root 4;part uuid $devtype $devnum:$devpart_root partuuidr;setenv bootargs console=ttyAMA0,115200 earlycon=pl011,mmio32,0x21c0000 root=PARTUUID=$partuuidr rw rootwait pci=pcie_bus_perf $othbootargs;load $devtype $devnum:$devpart_boot $kernel_addr_r $kernel_image;load $devtype $devnum:$devpart_boot $fdt_addr_r $dtb;env exists secureboot && echo validating secureboot && run secureboot_validate;booti $kernel_addr_r - $fdt_addr_r