LX2080A XSPI_A interface topology inquire

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LX2080A XSPI_A interface topology inquire

310 Views
Rex4_Huang
Contributor I

Hi Sir,

I have two SPI devices on our board,

one is an XSPI flash for NXP U-BOOT & KERNAL use, and the other one is a QSPI device.  

Q1.Can I use XSPI_A of LX2080A to connect them?

Q2. Can these devices be worked together?

the simple connection topology is shown as below:

Rex4_Huang_0-1705634472875.png

 

0 Kudos
Reply
1 Reply

259 Views
yipingwang
NXP TechSupport
NXP TechSupport

A1. The connection looks fine. However, the SW need to know one is 8 bit data line vs 4 data lines.
A2. I do not know what do you mean whether these devices can be worked together? The commands send to these two flashes should be different as one should be x8 another should be x4.

0 Kudos
Reply