LS1046ARDB NET-SNMP service cross-compile

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046ARDB NET-SNMP service cross-compile

1,683 Views
Ghouse
Contributor V

I have build net-snmp in ubantu 18.04.

./configure using cross compiler fsl-qoriql arrch64-fsl-linux-gnu, i am able to run service in ubuntu 18.04 successfully, but target machine is showing

./snmpd -d -f -L

warning: no access control information configured

[config search path: /ncs/etc/snmp:/ncs/share/snmp:/ncs/lib/snmp:/root/.snmp]

Run snmpconf -g basic-setup to help you configure the snmpd.conf file for this agent.

service is started but I am not able to get the agent response in client side here are the attached screenshots. 

please help to get it sort it out.

0 Kudos
2 Replies

1,653 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please run the following command to configure and generate snmpd.conf in /ncs/share/snmp

$cd /ncs

$ perl ./bin/snmpconf -i

Please refer to the following link to configure snmpd.conf file for the agent.

https://kb.juniper.net/InfoCenter/index?page=content&id=KB25949

Then run command

./sbin/snmpd -d -f -L

0 Kudos

1,682 Views
Ghouse
Contributor V

leftover screenshots are here... please refer it. maximum 5 only i can share so here attached remaining.

0 Kudos