LS1046ARDB KIT EEPROM READ AND WRITE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1046ARDB KIT EEPROM READ AND WRITE

972 次查看
IB2020
Contributor II

i was trying to read and write data bytes to EEPROM CAT24C05. It is not working.I could open the i2c  interface with slave address 52 .After that writing address byte is not happening.

0 项奖励
回复
3 回复数

966 次查看
ufedor
NXP Employee
NXP Employee

Please provide log of the performed operations.

Please consider that the SEEPROM contains important system information (like MAC addresses), so it has to be handled accurately.

0 项奖励
回复

952 次查看
IB2020
Contributor II

The source code is attached .I could open the eeprom i2c interface.But after that fail to write i2c address errror is coming. Kindly help. Also i would like to know which address locations MAC address and other important data is stored.

0 项奖励
回复

946 次查看
ufedor
NXP Employee
NXP Employee

For the I2C source code refer to the U-Boot driver:

drivers/i2c/mxc_i2c.c
0 项奖励
回复