I have a USB stick with FAT32 filesystem. When I attach it to LS1043ARDB and run "usb start" from U-Boot prompt the device resets/reboots with "Unexpected XHCI event TRB, skipping" message.
Why do I see this error? Is there a workaround to fix this?
=> usb start
starting USB...
Bus usb3@2f00000: Register 200017f NbrPorts 2
Starting the controller
USB XHCI 1.00
Bus usb3@3000000: Register 200017f NbrPorts 2
Starting the controller
USB XHCI 1.00
Bus usb3@3100000: Register 200017f NbrPorts 2
Starting the controller
USB XHCI 1.00
scanning bus usb3@2f00000 for devices... WARN halted endpoint, queueing URB anyway.
Unexpected XHCI event TRB, skipping... (f7b0b3b0 00000000 13000000 01008401)
BUG at drivers/usb/host/xhci-ring.c:503/abort_td()!
BUG!
resetting ...
Hello, I have the same issue and I really want to know why this is happening. The workaround of commenting these 3 lines is working for my current U-Boot, but after checking for the latest version, it seems these lines are still in the latest uboot.
Here my current U-Boot of NXP.
=> version
U-Boot 2022.07 (Jan 01 1970 - 01:00:00 +0000)
Yes, here is how I fix it:
1) find file common/usb_storage.c
2) go to function static int usb_stor_probe_device(struct usb_device *udev)
3) remark out following 3 line of code:
...
/* Comment our following function call because it causes usb endpoints halt
ret = blk_probe_or_unbind(dev)
if(ret)
return ret;
*/
...