I make DDR4 validation on LS1043ARDB by CodeWarrior QCVS, DDR controller register value get from u-boot-2016.11, But all validation failed. Failed tips: DDR initalization failed: D_INIT was not cleared by hardware!
Is CodeWarriro config error or register config error? Can you give me a right config project that used in CodeWarrior Development Studio for QorIQ LS series.
Original Attachment has been moved to: LS1043A_v1_0_codewarrior_regs.regs.zip
Hi 张洪军 张 ,\
I also have encountered same issue..
when i run the validation it was showing error like:
Error configuring the target! - DDR initialization failed: D_INIT was not cleared by hardware!>>
https://community.nxp.com/message/973994
How didi you resolve this issue? Help me in this ..
Regards,
suresh
How did you get the value of DDR regs from UBoot? The easy way to to that is to stop uboot at prompt then from QCVS to use Import From Target (You can find this option under File format in Import tab).
Also, as a reference you can use attached configuration for LS1043ARBD (got to Import tab, select File format Annotated Hex Text and import the file).
Adrian