Is there any information/changelog about CPLD firmware?
We found out, a before posted issue about GPIO1_DAT25 irq line behaviour depends on CPLD firmware version. With rev. 6 of firmware the posted solution works fine, with currently shipped version rev. 8 not. With rev. 8 we can't get any irq on line GPIO1_DAT25.
Flashing back to rev 6 works for irq issue, but we don't know what other issues or function were changed or fixed with rev 8.
Using mikroBUS INT Pin (GPIO1_DAT25) as trigger for gpiod based application on LS128ARDB-PA
fedor,
i assume CTL[5] ist ment to be "general control" register of QIXIS configuration.
Is it possible to configure bit 5 during bootup to enable the PIC e.g. patching the QIXIS init inside uboot?
What about the registers for:
POLARITY
EDGE/LEVEL
MASK
STAT
Where can i configure/read them?
fedor,
thanks a lot for your quick response. The release notes are very helpful!
One thing i need to know about [E30]
Which configuration do i have to do for activating the PIC?
What does CTL[5] mean? is it part of BRDCFG (QIXIS) or part of RCW?