Greetings,
I am building SDK v1.8 for the LS1021A TWR board, using GCC 4.8.4. I modified the U-Boot environment to boot via TFTP. eTSEC2 and 3 work, but eTSEC1 cannot communicate. It establishes link at 1Gbps, however I never see Tx packets show up at the switch. eTSEC1 sets up as eth0 in Linux, but does not work there either.
I verified that the HW is using NOR flash 0 RCW and that RCW is SSR_PPN_20. SW2 and SW3 are at defaults.
Is there something I must do in order to get all 3 network interfaces functional? What further information can I provide?
Thank you,
Maury Anderson
解決済! 解決策の投稿を見る。
Hello Maury Anderson,
According to your u-boot log, it seems that you use RCW RSR_PPS_70/rcw_1000.bin, the setting of this RCW is 1 SGMII, 1 RGMII, 1SATA, 2PCIE, CAN, SAI, please refer to the the following SerDes options, that's why eTSEC1 cannot work. Please use RCW SSR_PPN_20/rcw_1000.bin in the pre-built image ISO, and please make sure that you flash the RCW on the correct bank.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Maury Anderson,
Do you use LS1021ATWR CPU Rev1.0 or Rev2.0 board?
Would you please provide u-boot and Linux Kernel boot log?
Please setup eth0 and provide the result of "ethtool eth0".
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Greetings Yiping,
Thank you for your response. Here is my attempt to satisfy the request for information. I have doubts, based on ethtool information, that we are using eTSEC1 in a valid way.
Thanks for your help,
Maury
############################################################
Revision Data
############################################################
Silkscreen on circuit card is: (c) 2014 LS-1021A
There are 3 labels on circuit card containing revision details:
700-28040 REV C
SCH-28040 REV D1
CPLD v2.3 LS1021A SDK v1.3
############################################################
Boot Output
############################################################
U-Boot 2015.01-RCLinux-NewShinyDevKit (Sep 09 2015 - 13:23:58)
CPU: Freescale LayerScape LS1021E, Version: 1.0, (0x87081110)
Clock Configuration:
CPU0(ARMV7):1000 MHz,
Bus:300 MHz, DDR:800 MHz (1600 MT/s data rate),
Reset Configuration Word (RCW):
00000000: 0608000a 00000000 00000000 00000000
00000010: 70000000 00407900 e0025a00 21046000
00000020: 00000000 00000000 00000000 00038000
00000030: 00080000 48007340 00000000 00000000
Board: LS1021ATWR
CPLD: V2.3
PCBA: V4.0
VBank: 0
I2C: ready
DRAM: 1 GiB
Using SERDES1 Protocol: 112 (0x70)
Firmware 'Microcode version 0.0.0 for T1040 r1.0' for 1040 V1.0
QE: uploading microcode 'Microcode for T1040 r1.0'
Flash: 128 MiB
MMC: FSL_SDHC: 0
EEPROM: CRC mismatch (3b162798 != ffffffff)
PCIe1: Root Complex no link, regs @ 0x3400000
PCIe2: Root Complex no link, regs @ 0x3500000
In: serial
Out: serial
Err: serial
SEC0: RNG instantiated
SATA link 0 timeout.
AHCI 0001.0300 1 slots 1 ports ? Gbps 0x1 impl SATA mode
flags: 64bit ncq pm clo only pmp fbss pio slum part ccc
scanning bus for devices...
Found 0 device(s).
SCSI: Net: eTSEC2 is in sgmii mode.
eTSEC1 [PRIME], eTSEC2, eTSEC3
Hit any key to stop autoboot: 0
eTSEC1 Waiting for PHY auto negotiation to complete. done
Speed: 1000, full duplex
Using eTSEC1 device
TFTP from server 10.10.0.1; our IP address is 10.10.0.100
Filename 'ls1021twr0/uImage'.
Load address: 0x80020000
Loading: T T T T T T T T T T
Retry count exceeded; starting again
Speed: 1000, full duplex
Using eTSEC2 device
TFTP from server 10.10.0.1; our IP address is 10.10.0.100
Filename 'ls1021twr0/ls1021a-twr.dtb'.
Load address: 0x80000000
Loading: ##
1.5 MiB/s
done
Bytes transferred = 21046 (5236 hex)
Speed: 1000, full duplex
Using eTSEC2 device
TFTP from server 10.10.0.1; our IP address is 10.10.0.100
Filename 'ls1021twr0/rootfs.cpio.uboot'.
Load address: 0x81000000
Loading: #################################################################
#################################################################
#################################################################
#################################################################
################################
1.7 MiB/s
done
Bytes transferred = 4279911 (414e67 hex)
## Booting kernel from Legacy Image at 80020000 ...
Image Name: Linux-3.12.37-rt51-RCLinux-Maury
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3105160 Bytes = 3 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
## Loading init Ramdisk from Legacy Image at 81000000 ...
Image Name:
Image Type: ARM Linux RAMDisk Image (uncompressed)
Data Size: 4279847 Bytes = 4.1 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
## Flattened Device Tree blob at 80000000
Booting using the fdt blob at 0x80000000
Loading Kernel Image ... OK
Loading Ramdisk to beb0f000, end bef23e27 ... OK
Loading Device Tree to beb06000, end beb0e235 ... OK
Starting kernel ...
i2c i2c-2: of_i2c: modalias failure on /soc/i2c@21a0000/ltc2945@67
layerscape-pcie 3400000.pcie: phy link never came up
layerscape-pcie 3500000.pcie: phy link never came up
sgtl5000 1-000a: Failed to get supply 'VDDD': -19
drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
Starting logging: OK
Initializing random number generator... done.
Starting network...
udhcpc (v1.23.1) started
Sending discover...
Sending discover...
Sending discover...
Sending select for 10.10.1.74...
Lease of 10.10.1.74 obtained, lease time 86400
adding dns 10.10.0.1
Welcome to Linux
devkit login:
############################################################
Ethtool Output
############################################################
# ethtool eth0
Settings for eth0:
Supported ports: [ MII ]
Supported link modes: 10baseT/Half 10baseT/Full
100baseT/Half 100baseT/Full
1000baseT/Full
Supported pause frame use: Symmetric Receive-only
Supports auto-negotiation: Yes
Advertised link modes: 10baseT/Half 10baseT/Full
100baseT/Half 100baseT/Full
1000baseT/Full
Advertised pause frame use: No
Advertised auto-negotiation: Yes
Speed: 1000Mb/s
Duplex: Full
Port: MII
PHYAD: 2
Transceiver: external
Auto-negotiation: on
Supports Wake-on: uag
Wake-on: d
Current message level: 0x0000003f (63)
drv probe link timer ifdown ifup
Link detected: yes
#
Hello Maury Anderson,
According to your u-boot log, it seems that you use RCW RSR_PPS_70/rcw_1000.bin, the setting of this RCW is 1 SGMII, 1 RGMII, 1SATA, 2PCIE, CAN, SAI, please refer to the the following SerDes options, that's why eTSEC1 cannot work. Please use RCW SSR_PPN_20/rcw_1000.bin in the pre-built image ISO, and please make sure that you flash the RCW on the correct bank.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Based on this tab, I wonder how can I use eTSEC0 as SGMII , eTSEC1 and eTSEC2 as RGMII, it seems like SGMII1 and SGMII2 must be configured at the same time
I am facing same issue i.e eTSEC1 is not working while eTSEC2 and eTSEC3 are working. I have posted this in below thread.
https://community.nxp.com/thread/439364
Any help is highly appreciated.
Hi Romit, I posted comment here, where I described that I think the MUX is improperly switched. Noone said I am wrong, noone posted a CPLD source matching the label on our Tower board.
Hi Dusan,
Thanks for your reply. I think MUX is properly switched and also according to board specification (TWR-LS1021ARM), eTSEC ports do not depend on any switch setting.
Are you still facing this issue of eTSEC1 not working while eTSEC2 and eTSEC3 are working? Have you found any solution?
Hi,
I see this is relevant thread to post my rcw_1000.rcw recompilation issue.
My custom board is bit different than the reference board LS1021TWR, so i have modified the RCW bits according to my board using CW dev studio+QCVS tool and using it.
I want to include this as part of Yocto tree and build it along with other images(linux kernel,u-boot,RFS etc).
So i had generated pbl.pbl file from CW dev studio and modified rcw_1000.rcw file under /rcw/git-r0/git/nextflash/SSR_PNS_30/ path,but the issue is only when i do the cleanstate build using bitbake it builds this file else it will not recompile this file.
If someone is aware of how to recompile without doing cleanstate with bitbake(as it takes nearly 1 hour to recompile the tree),kindly help me out.
Best Regards,
Nagi