Hi,
I am having LS1021AIOT board, (LS1021A Rev 1.0, IOT boar Rev X2).
The Realtek RTL8365MB 4+1 port Gigabit ethernet Switch in connected in eth2 (eTSEC3).
SDK is Yocto (QorIQ-SDK-V1.8).
I cannot communicate through the switch on this reference board with this code. ie, LS1021AIOT eTSEC3 - RTL8365 ethernet switch not working.
The RCW for eth3 is set for RGMII (000). In the Dts file in kernel, eth2 was set as rgmii-id, and in gianfar.c it was checking only rgmii. I have changed it.
Now on booting, it is verified that code runs through "Configuring RGMII mode" in gianfar.c. If I up/down eth2, it gets configured as RGMII (code runs, not sure whether PHY actually configured).
I can ping from on device connected to this switch to another device connected in the same switch. But I cannot communicate with other network.
brctl showstp br-lan command shows:
root@OpenWrt:~# brctl showstp br-lan
br-lan
bridge id 7fff.001f7b6301aa
designated root 7fff.001f7b6301aa
root port 0 path cost 0
max age 20.00 bridge max age 20.00
hello time 2.00 bridge hello time 2.00
forward delay 2.00 bridge forward delay 2.00
ageing time 300.00
hello timer 0.64 tcn timer 0.00
topology change timer 0.00 gc timer 117.76
flags
eth0
port id 8001 state disabled
designated root 7fff.001f7b6301aa path cost 4
designated bridge 7fff.001f7b6301aa message age timer 0.00
designated port 8001 forward delay timer 0.00
designated cost 0 hold timer 0.00
flags
eth1
port id 8002 state disabled
designated root 7fff.001f7b6301aa path cost 100
designated bridge 7fff.001f7b6301aa message age timer 0.00
designated port 8002 forward delay timer 0.00
designated cost 0 hold timer 0.00
flags
The default br-lan bridge interface is up by default, and both eth0 and eth1 is added as shown above. I cannot ping from eth0 or eth1 to this eth2 How this can be resolved ?
解決済! 解決策の投稿を見る。
Hi Pavel,
We have solved the issue, the issue was with RTL switch initialization. The SDK provided with the reference board was not initializing the RTL switch, so we integrated user space application for configuring the RTL Switch over DSPI, now its working.
It looks like that configuration of your network is incorrect. It looks like that gateway and DNS server is not defined for your board.
Have a great day,
Pavel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Pavel,
We have solved the issue, the issue was with RTL switch initialization. The SDK provided with the reference board was not initializing the RTL switch, so we integrated user space application for configuring the RTL Switch over DSPI, now its working.
Hi
I have the same problem, where you change RTL switch initialization? I can't find this in the current SDK?
this SDk https://nxp.flexnetoperations.com/control/frse/product?child_plneID=684021&cert_num=727175607&ver=AR... support LS1021A-IOT board?
Hi Pavel Chubakov,
As per the documentation available on Freescale Website, (http://cache.nxp.com/files/soft_dev_tools/doc/support_info/LS1021A-SDK-V1.1-ARM-SOURCE_RMF.txt?fpsp=... ) about RTL L2 switch, it is saying that:
"The RTL L2 switch will be initialized on boot, the interface name is "eth2", use below command to add it to bridge:
$ ifconfig eth2 up
$ brctl addif br-lan eth2"
I have done the step.
If I run 'ethtool eth2' command on fsl-image-rds, I am getting the below :
# ethtool eth2
Settings for eth2:
Supported ports: [ MII ]
Supported link modes: 10baseT/Half 10baseT/Full
100baseT/Half 100baseT/Full
1000baseT/Full
Supported pause frame use: Symmetric Receive-only
Supports auto-negotiation: Yes
Advertised link modes: 10baseT/Half 10baseT/Full
100baseT/Half 100baseT/Full
1000baseT/Full
Advertised pause frame use: No
Advertised auto-negotiation: Yes
Speed: 1000Mb/s
Duplex: Full
Port: MII
PHYAD: 2
Transceiver: external
Auto-negotiation: off
Supports Wake-on: g
Wake-on: d
Current message level: 0x0000003f (63)
drv probe link timer ifdown ifup
Link detected: yes
It shows the eth2 is configured in MII.
I am using LS1021A-IoT Gateway Reference Design SDK Source ISO (REV 1.8).The Hardware is configured for RGMII, and in device tree by default it was initializing as MII only, not RGMII. I have change it to rgmii-id now, and on booting, I gets prints of eth2 configured in RGMII. Still on 'ethtool eth2' command, I am getting MII only. What could be the problem ?