LS1012ARDB SDK V0.5 don't mount EMMC Root File System

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1012ARDB SDK V0.5 don't mount EMMC Root File System

1,543 次查看
jasonwu0527
Contributor I

I can't mount EMMC Root File System.I refer to SDK 2.0 inittab entries not found booting from /dev/mmcblk0p2 and  QorIQ LS1012A BSP v0.5 Guide, but does not working.

001.jpg

002.jpg

Error log as follows:

root@ls1012ardb:~# ls -alh /run/media/mmcblk1
total 37M
drwxr-xr-x 19 root root 4.0K Dec 28 07:34 .
drwxr-xr-x 4 root root 80 Jan 1 1970 ..
drwxr-xr-x 2 root root 4.0K Dec 28 07:37 bin
drwxr-xr-x 2 root root 4.0K Dec 28 07:36 boot
drwxr-xr-x 2 root root 4.0K Apr 26 08:47 dev
drwxr-xr-x 65 root root 4.0K Dec 28 07:37 etc
drwxr-xr-x 3 root root 4.0K Dec 28 07:35 home
-rwxr-x--- 1 root root 37M Dec 28 07:34 kernel-ls1012ardb.itb
drwxr-xr-x 10 root root 4.0K Dec 28 07:37 lib
lrwxrwxrwx 1 root root 12 Dec 28 07:36 linuxrc -> /bin/busybox
drwx------ 2 root root 16K May 10 2017 lost+found
drwxr-xr-x 2 root root 4.0K Apr 26 08:47 media
drwxr-xr-x 2 root root 4.0K Apr 26 08:47 mnt
drwxr-xr-x 3 root root 4.0K Dec 28 07:37 opt
drwxr-xr-x 2 root root 4.0K Apr 26 08:47 proc
drwxr-xr-x 3 root root 4.0K Dec 28 07:36 run
drwxr-xr-x 2 root root 4.0K Dec 28 07:37 sbin
drwxr-xr-x 2 root root 4.0K Apr 26 08:47 sys
drwxrwxrwt 2 root root 4.0K Apr 26 08:47 tmp
drwxr-xr-x 10 root root 4.0K Dec 28 07:37 usr
drwxr-xr-x 11 root root 4.0K Dec 28 07:37 var

=> printenv
baudrate=115200
boot_bank1=i2c mw 0x24 0x3 0xf4;reset
boot_bank2=i2c mw 0x24 0x7 0xfc; i2c mw 0x24 0x3 0xf5;reset
bootargs=root=/dev/mmcblk1 rw earlycon=uart8250,0x21c0500 console=ttyS0,115200
bootcmd=ext2load mmc 1 a0000000 kernel-ls1012ardb.itb && bootm a0000000
bootdelay=5
console=ttyS0,115200
eth0addr=00:04:9f:04:68:b0
eth1addr=00:04:9f:04:68:b1
eth2addr=00:04:9f:04:68:b2
ethact=pfe_eth0
ethaddr=00:04:9f:04:68:b3
fdt_high=0xffffffffffffffff
fdtcontroladdr=bfc7a348
fileaddr=90000000
filesize=2459807
hwconfig=fsl_ddr:bank_intlv=auto
initrd_high=0xffffffffffffffff
ipaddr=192.168.3.12
kernel_addr=0x100000
kernel_load=0xa0000000
kernel_size=0x2800000
kernel_start=0xa00000
loadaddr=0x80100000
ramdisk_addr=0x800000
ramdisk_size=0x2000000
scsidevs=0
serverip=192.168.3.1
stderr=serial
stdin=serial
stdout=serial
verify=no

Environment size: 893/262140 bytes

U-Boot 2016.01LS1012A-SDK+gc584f35 (Dec 28 2016 - 15:17:35 +0800)

SoC: LS1012AE (0x87040010)
Clock Configuration:
CPU0(A53):800 MHz
Bus: 250 MHz DDR: 1000 MT/s
Reset Configuration Word (RCW):
00000000: 08000008 00000000 00000000 00000000
00000010: 35080000 c000000c 40000000 00001800
00000020: 00000000 00000000 00000000 00014571
00000030: 00000000 18c2a120 00000096 00000000
I2C: ready
DRAM: 1022 MiB
SEC: RNG instantiated
Using SERDES1 Protocol: 13576 (0x3508)
MMC: FSL_SDHC: 0, FSL_SDHC: 1
SF: Detected S25FS512S_256K with page size 512 Bytes, erase size 256 KiB, total 64 MiB
PCIe1: Root Complex x1 gen1, regs @ 0x3400000
PCI:
01:00.0 - 168c:0030 - Network controller
PCIe1: Bus 00 - 01
In: serial
Out: serial
Err: serial
Model: LS1012A RDB Board
Board: LS1012ARDB Version: RevB, boot from QSPI: bank2
SATA link 0 timeout.
AHCI 0001.0301 32 slots 1 ports 6 Gbps 0x1 impl SATA mode
flags: 64bit ncq pm clo only pmp fbss pio slum part ccc apst
Found 0 device(s).
SCSI: Net: cbus_baseaddr: 0000000004000000, ddr_baseaddr: 0000000083800000, ddr_phys_baseaddr: 03800000
class init complete
tmu init complete
bmu1 init: done
bmu2 init: done
GPI1 init complete
GPI2 init complete
HGPI init complete
hif_tx_desc_init: Tx desc_base: 0000000083e40400, base_pa: 03e40400, desc_count: 64
hif_rx_desc_init: Rx desc base: 0000000083e40000, base_pa: 03e40000, desc_count: 64
HIF tx desc: base_va: 0000000083e40400, base_pa: 03e40400
HIF init complete
bmu1 enabled
bmu2 enabled
pfe_hw_init: done
pfe_firmware_init
pfe_load_elf: no of sections: 13
pfe_firmware_init: class firmware loaded
pfe_load_elf: no of sections: 10
pfe_firmware_init: tmu firmware loaded
ls1012a_configure_serdes 0
pfe_eth0, pfe_eth1
Hit any key to stop autoboot: 0
38115335 bytes read in 2050 ms (17.7 MiB/s)
## Loading kernel from FIT Image at a0000000 ...
Using 'config@1' configuration
Trying 'kernel@1' kernel subimage
Description: ARM64 Linux kernel
Type: Kernel Image
Compression: uncompressed
Data Start: 0xa0000134
Data Size: 12534784 Bytes = 12 MiB
Architecture: AArch64
OS: Linux
Load Address: 0x80080000
Entry Point: 0x80080000
## Loading ramdisk from FIT Image at a0000000 ...
Using 'config@1' configuration
Trying 'ramdisk@1' ramdisk subimage
Description: Ramdisk
Type: RAMDisk Image
Compression: uncompressed
Data Start: 0xa0bf6e9c
Data Size: 25568799 Bytes = 24.4 MiB
Architecture: AArch64
OS: Linux
Load Address: unavailable
Entry Point: unavailable
## Loading fdt from FIT Image at a0000000 ...
Using 'config@1' configuration
Trying 'fdt@1' fdt subimage
Description: Flattened Device Tree blob
Type: Flat Device Tree
Compression: uncompressed
Data Start: 0xa0bf45e8
Data Size: 10291 Bytes = 10 KiB
Architecture: AArch64
Loading fdt from 0xa0bf45e8 to 0x90000000
Booting using the fdt blob at 0x90000000
Loading Kernel Image ... OK
Using Device Tree in place at 0000000090000000, end 0000000090005832

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Linux version 4.1.8-rt8+gb483089 (jason@ubuntu) (gcc version 4.9.4 20150629 (prerelease) (Linaro GCC 4.9-2015.06) ) #1 SMP Wed Apr 26 05:06:58 PDT 2017
[ 0.000000] CPU: AArch64 Processor [410fd034] revision 4
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] alternatives: enabling workaround for ARM erratum 845719
[ 0.000000] earlycon: Early serial console at MMIO 0x21c0500 (options '')
[ 0.000000] bootconsole [uart0] enabled
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] cma: Reserved 16 MiB at 0x00000000bec00000
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv0.2 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] WARNING: x1-x3 nonzero in violation of boot protocol:
[ 0.000000] x1: 0000000000000000
[ 0.000000] x2: 0000000000000000
[ 0.000000] x3: 0000000080080000
[ 0.000000] This indicates a broken bootloader or old kernel
[ 0.000000] PERCPU: Embedded 18 pages/cpu @ffff80003fdd4000 s33856 r8192 d31680 u73728
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 257544
[ 0.000000] Kernel command line: root=/dev/mmcblk1 rw earlycon=uart8250,0x21c0500 console=ttyS0,115200
[ 0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 8, 1048576 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 7, 524288 bytes)
[ 0.000000] software IO TLB [mem 0xb9a00000-0xbda00000] (64MB) mapped at [ffff800039a00000-ffff80003d9fffff]
[ 0.000000] Memory: 895764K/1046528K available (7859K kernel code, 577K rwdata, 3252K rodata, 476K init, 760K bss, 134380K reserved, 16384K cma-reserved)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vmalloc : 0xffff000000000000 - 0xffff7bffbfff0000 (126974 GB)
[ 0.000000] vmemmap : 0xffff7bffc0000000 - 0xffff7fffc0000000 ( 4096 GB maximum)
[ 0.000000] 0xffff7bffc2000000 - 0xffff7bffc2ff8000 ( 15 MB actual)
[ 0.000000] fixed : 0xffff7ffffabfd000 - 0xffff7ffffac00000 ( 12 KB)
[ 0.000000] PCI I/O : 0xffff7ffffae00000 - 0xffff7ffffbe00000 ( 16 MB)
[ 0.000000] modules : 0xffff7ffffc000000 - 0xffff800000000000 ( 64 MB)
[ 0.000000] memory : 0xffff800000000000 - 0xffff80003fe00000 ( 1022 MB)
[ 0.000000] .init : 0xffff800000b5c000 - 0xffff800000bd3000 ( 476 KB)
[ 0.000000] .text : 0xffff800000080000 - 0xffff800000b5bf64 ( 11120 KB)
[ 0.000000] .data : 0xffff800000be4000 - 0xffff800000c74400 ( 577 KB)
[ 0.000000] Hierarchical RCU implementation.
[ 0.000000] Additional per-CPU info printed with stalls.
[ 0.000000] RCU restricting CPUs from NR_CPUS=64 to nr_cpu_ids=1.
[ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1
[ 0.000000] NR_IRQS:64 nr_irqs:64 0
[ 0.000000] Architected cp15 timer(s) running at 25.00MHz (phys).
[ 0.000000] clocksource arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x5c40939b5, max_idle_ns: 440795202646 ns
[ 0.000004] sched_clock: 56 bits at 25MHz, resolution 40ns, wraps every 4398046511100ns
[ 0.008373] Console: colour dummy device 80x25
[ 0.012863] Calibrating delay loop (skipped), value calculated using timer frequency.. 50.00 BogoMIPS (lpj=250000)
[ 0.023309] pid_max: default: 32768 minimum: 301
[ 0.028039] Security Framework initialized
[ 0.032212] Mount-cache hash table entries: 2048 (order: 2, 16384 bytes)
[ 0.038967] Mountpoint-cache hash table entries: 2048 (order: 2, 16384 bytes)
[ 0.046709] Initializing cgroup subsys memory
[ 0.051126] Initializing cgroup subsys hugetlb
[ 0.055806] hw perfevents: enabled with arm/armv8-pmuv3 PMU driver, 7 counters available
[ 0.064012] EFI services will not be available.
[ 0.069334] Brought up 1 CPUs
[ 0.072323] SMP: Total of 1 processors activated.
[ 0.077085] CPU: All CPU(s) started at EL2
[ 0.081221] alternatives: patching kernel code
[ 0.086117] devtmpfs: initialized
[ 0.091944] DMI not present or invalid.
[ 0.096000] clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.106890] pinctrl core: initialized pinctrl subsystem
[ 0.113200] NET: Registered protocol family 16
[ 0.118589] cpuidle: using governor ladder
[ 0.122721] cpuidle: using governor menu
[ 0.126739] fsl-mc bus type registered
[ 0.130597] MC object device driver fsl_mc_dprc registered
[ 0.136152] MC object device driver fsl_mc_allocator registered
[ 0.142310] vdso: 2 pages (1 code @ ffff800000be9000, 1 data @ ffff800000be8000)
[ 0.149801] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.159428] DMA: preallocated 256 KiB pool for atomic allocations
[ 0.165755] Serial: AMBA PL011 UART driver
[ 0.199632] RCPM: layerscape_rcpm_init: The RCPM driver initialized.
[ 0.208698] vgaarb: loaded
[ 0.211695] SCSI subsystem initialized
[ 0.216204] usbcore: registered new interface driver usbfs
[ 0.221783] usbcore: registered new interface driver hub
[ 0.227186] usbcore: registered new device driver usb
[ 0.232786] i2c i2c-0: IMX I2C adapter registered
[ 0.237542] i2c i2c-0: can't use DMA
[ 0.241231] pps_core: LinuxPPS API ver. 1 registered
[ 0.246231] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.255466] PTP clock support registered
[ 0.259652] No BMan portals available!
[ 0.265256] QMan: Allocated lookup table at ffff000000151000, entry count 65537
[ 0.272824] No QMan portals available!
[ 0.276777] No USDPAA memory, no 'fsl,usdpaa-mem' in device-tree
[ 0.283085] Advanced Linux Sound Architecture Driver Initialized.
[ 0.290358] Switched to clocksource arch_sys_counter
[ 0.307954] NET: Registered protocol family 2
[ 0.312900] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.320131] TCP bind hash table entries: 8192 (order: 5, 131072 bytes)
[ 0.326889] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.333410] UDP hash table entries: 512 (order: 2, 16384 bytes)
[ 0.339404] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[ 0.346003] NET: Registered protocol family 1
[ 0.351286] RPC: Registered named UNIX socket transport module.
[ 0.357258] RPC: Registered udp transport module.
[ 0.362030] RPC: Registered tcp transport module.
[ 0.366767] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.373453] Trying to unpack rootfs image as initramfs...
[ 0.379291] rootfs image is not initramfs (no cpio magic); looks like an initrd
[ 0.464876] Freeing initrd memory: 24968K (ffff800020bf7000 - ffff800022459000)
[ 0.472510] hw perfevents: Failed to parse /pmu/interrupt-affinity[0]
[ 0.479286] kvm [1]: interrupt-controller@1404000 IRQ6
[ 0.484962] kvm [1]: timer IRQ3
[ 0.488128] kvm [1]: Hyp mode initialized successfully
[ 0.495582] futex hash table entries: 256 (order: 2, 16384 bytes)
[ 0.501872] audit: initializing netlink subsys (disabled)
[ 0.507361] audit: type=2000 audit(0.430:1): initialized
[ 0.513973] HugeTLB registered 2 MB page size, pre-allocated 0 pages
[ 0.520993] VFS: Disk quotas dquot_6.6.0
[ 0.524990] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.532656] NFS: Registering the id_resolver key type
[ 0.537775] Key type id_resolver registered
[ 0.542020] Key type id_legacy registered
[ 0.546285] fuse init (API version 7.23)
[ 0.550858] 9p: Installing v9fs 9p2000 file system support
[ 0.557526] async_tx: api initialized (async)
[ 0.561996] io scheduler noop registered
[ 0.566004] io scheduler cfq registered (default)
[ 0.572184] PCI host bridge /soc/pcie@3400000 ranges:
[ 0.577292] IO 0x4000010000..0x400001ffff -> 0x00000000
[ 0.582850] MEM 0x4040000000..0x407fffffff -> 0x40000000
[ 0.588549] layerscape-pcie 3400000.pcie: PCI host bridge to bus 0000:00
[ 0.595320] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 0.600859] pci_bus 0000:00: root bus resource [io 0x0000-0xffff]
[ 0.607091] pci_bus 0000:00: root bus resource [mem 0x4040000000-0x407fffffff] (bus address [0x40000000-0x7fffffff])
[ 0.630125] pci 0000:00:00.0: BAR 8: assigned [mem 0x4040000000-0x40400fffff]
[ 0.637330] pci 0000:00:00.0: BAR 6: assigned [mem 0x4040100000-0x40401007ff pref]
[ 0.644989] pci 0000:01:00.0: BAR 0: assigned [mem 0x4040000000-0x404001ffff 64bit]
[ 0.652767] pci 0000:01:00.0: BAR 6: assigned [mem 0x4040020000-0x404002ffff pref]
[ 0.660408] pci 0000:00:00.0: PCI bridge to [bus 01]
[ 0.665414] pci 0000:00:00.0: bridge window [mem 0x4040000000-0x40400fffff]
[ 0.672911] pcieport 0000:00:00.0: Signaling PME through PCIe PME interrupt
[ 0.679942] pci 0000:01:00.0: Signaling PME through PCIe PME interrupt
[ 0.687203] Freescale LS2 console driver
[ 0.691822] fsl-ls2-console: device fsl_mc_console registered
[ 0.697791] fsl-ls2-console: device fsl_aiop_console registered
[ 0.709022] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled
[ 0.717426] msm_serial: driver initialized
[ 0.722409] console [ttyS0] disabled
[ 0.726049] 21c0500.serial: ttyS0 at MMIO 0x21c0500 (irq = 14, base_baud = 7812500) is a 16550A
[ 0.734880] console [ttyS0] enabled
[ 0.734880] console [ttyS0] enabled
[ 0.741887] bootconsole [uart0] disabled
[ 0.741887] bootconsole [uart0] disabled
[ 0.750568] 21c0600.serial: ttyS1 at MMIO 0x21c0600 (irq = 14, base_baud = 7812500) is a 16550A
[ 0.760496] Unable to detect cache hierarcy from DT for CPU 0
[ 0.776437] brd: module loaded
[ 0.784504] loop: module loaded
[ 0.788362] ahci-qoriq 3200000.sata: AHCI 0001.0301 32 slots 1 ports 6 Gbps 0x1 impl platform mode
[ 0.797405] ahci-qoriq 3200000.sata: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc sds apst
[ 0.808867] scsi host0: ahci-qoriq
[ 0.812577] ata1: SATA max UDMA/133 mmio [mem 0x03200000-0x0320ffff] port 0x100 irq 19
[ 0.822419] fsl-quadspi 1550000.quadspi: s25fl512s (65536 Kbytes)
[ 0.830623] tun: Universal TUN/TAP device driver, 1.6
[ 0.835688] tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>
[ 0.844000] Freescale FM module, FMD API version 21.1.0
[ 0.849360] Freescale FM Ports module
[ 0.853084] fsl_mac: fsl_mac: FSL FMan MAC API based driver
[ 0.858764] fsl_dpa: FSL DPAA Ethernet driver
[ 0.863209] fsl_advanced: FSL DPAA Advanced drivers:
[ 0.868185] fsl_proxy: FSL DPAA Proxy initialization driver
[ 0.873843] fsl_dpa_shared: FSL DPAA Shared Ethernet driver
[ 0.879491] fsl_dpa_macless: FSL DPAA MACless Ethernet driver
[ 0.885324] fsl_oh: FSL FMan Offline Parsing port driver
[ 0.890736] e1000: Intel(R) PRO/1000 Network Driver - version 7.3.21-k8-NAPI
[ 0.897794] e1000: Copyright (c) 1999-2006 Intel Corporation.
[ 0.903629] e1000e: Intel(R) PRO/1000 Network Driver - 2.3.2-k
[ 0.909468] e1000e: Copyright(c) 1999 - 2014 Intel Corporation.
[ 0.915467] sky2: driver version 1.30
[ 0.920670] VFIO - User Level meta-driver version: 0.3
[ 0.926268] vfio_fsl_mc_driver_init: Driver registration fails as no fsl_mc_bus found
[ 1.335543] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 1.341084] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
[ 1.349767] xhci-hcd xhci-hcd.0.auto: hcc params 0x0220f66d hci version 0x100 quirks 0x00010010
[ 1.358580] xhci-hcd xhci-hcd.0.auto: irq 22, io mem 0x02f00000
[ 1.365414] hub 1-0:1.0: USB hub found
[ 1.369308] hub 1-0:1.0: 1 port detected
[ 1.373573] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 1.379078] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
[ 1.386984] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[ 1.395732] hub 2-0:1.0: USB hub found
[ 1.399620] hub 2-0:1.0: 1 port detected
[ 1.404057] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.410625] ehci-pci: EHCI PCI platform driver
[ 1.415151] ehci-platform: EHCI generic platform driver
[ 1.420561] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[ 1.426772] ohci-pci: OHCI PCI platform driver
[ 1.431286] ohci-platform: OHCI generic platform driver
[ 1.436703] usbcore: registered new interface driver usb-storage
[ 1.443676] mousedev: PS/2 mouse device common for all mice
[ 1.449925] i2c /dev entries driver
[ 1.454682] qoriq_cpufreq: Freescale QorIQ CPU frequency scaling driver
[ 1.461450] sdhci: Secure Digital Host Controller Interface driver
[ 1.467638] sdhci: Copyright(c) Pierre Ossman
[ 1.472053] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.478295] ata1: SATA link down (SStatus 0 SControl 300)
[ 1.484330] sdhci-esdhc 1560000.esdhc: No vmmc regulator found
[ 1.490218] sdhci-esdhc 1560000.esdhc: No vqmmc regulator found
[ 1.529994] mmc0: SDHCI controller on 1560000.esdhc [1560000.esdhc] using ADMA 64-bit
[ 1.540170] sdhci-esdhc 1580000.esdhc: No vmmc regulator found
[ 1.546016] sdhci-esdhc 1580000.esdhc: No vqmmc regulator found
[ 1.589994] mmc1: SDHCI controller on 1580000.esdhc [1580000.esdhc] using ADMA 64-bit
[ 1.599455] caam 1700000.crypto: Instantiated RNG4 SH1
[ 1.604666] caam 1700000.crypto: device ID = 0x0a14040000000000 (Era 8)
[ 1.611307] caam 1700000.crypto: job rings = 4, qi = 0
[ 1.623869] caam 1700000.crypto: caam memcpy support with 4 job rings
[ 1.633411] caam algorithms registered in /proc/crypto
[ 1.640096] caam_jr 1710000.jr: registering rng-caam
[ 1.645331] caam 1700000.crypto: fsl,sec-v5.4 algorithms registered in /proc/crypto
[ 1.653101] MC object device driver fsl_dpaa2_caam registered
[ 1.659471] usbcore: registered new interface driver usbhid
[ 1.665074] usbhid: USB HID core driver
[ 1.670197] fsl-mc bus not found, restool driver registration failed
[ 1.676638] MC object device driver fsl_dpio_drv registered
[ 1.682566] No fsl,qman node
[ 1.685626] Freescale USDPAA process driver
[ 1.689812] fsl-usdpaa: no region found
[ 1.693675] Freescale USDPAA process IRQ driver
[ 1.699989] MC object device driver fsl_dpaa2_eth registered
[ 1.705708] MC object device driver dpaa2_mac registered
[ 1.711076] MC object device driver dpaa2_ethsw registered
[ 1.716599] MC object device driver dpaa2_evb registered
[ 1.721960] MC object device driver fsl_dce_api registered
[ 1.727482] MC object device driver dpaa2_rtc registered
[ 1.738544] Initializing XFRM netlink socket
[ 1.742972] NET: Registered protocol family 10
[ 1.748447] sit: IPv6 over IPv4 tunneling driver
[ 1.753678] NET: Registered protocol family 17
[ 1.758150] NET: Registered protocol family 15
[ 1.762672] 8021q: 802.1Q VLAN Support v1.8
[ 1.766899] 9pnet: Installing 9P2000 support
[ 1.771260] Key type dns_resolver registered
[ 1.776828] registered taskstats version 1
[ 1.781541] fsl_generic: FSL DPAA Generic Ethernet driver
[ 1.787143] hctosys: unable to open rtc device (rtc0)
[ 1.792744] ALSA device list:
[ 1.795713] No soundcards found.
[ 1.800809] RAMDISK: gzip image found at block 0
[ 1.818450] mmc1: MAN_BKOPS_EN bit is not set
[ 1.837335] mmc1: new high speed MMC card at address 0001
[ 1.850633] mmcblk0: mmc1:0001 P1XXXX 3.60 GiB
[ 1.860450] mmcblk0boot0: mmc1:0001 P1XXXX partition 1 2.00 MiB
[ 1.870532] mmcblk0boot1: mmc1:0001 P1XXXX partition 2 2.00 MiB
[ 1.890608] mmcblk0rpmb: mmc1:0001 P1XXXX partition 3 128 KiB
[ 3.827914] VFS: Mounted root (ext2 filesystem) on device 1:0.
Bad inittab entry at line 5
can't open /dev/si: No such file or directory
can't open /dev/~~: No such file or directory
can't open /dev/l0: No such file or directory
can't open /dev/l1: No such file or directory
can't open /dev/l2: No such file or directory
can't open /dev/l3: No such file or directory
can't open /dev/l4: No such file or directory
can't open /dev/l5: No such file or directory
can't open /dev/l6: No such file or directory
can't open /dev/z6: No such file or directory
can't open /dev/S0: No such file or directory
can't open /dev/AMA0: No such file or directory
can't open /dev/z6: No such file or directory
can't open /dev/S0: No such file or directory
can't open /dev/AMA0: No such file or directory

标签 (1)
0 项奖励
回复
1 回复

822 次查看
Pavel
NXP Employee
NXP Employee

It looks like that u-boot should be changed on your board.

Use u-boot from your SDK.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复