LS1012A SDHC1 EMMC problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1012A SDHC1 EMMC problem

3,587件の閲覧回数
233158343
Contributor I

Hi NXP Team,

 

We are designing LS1012A(LS1012AXN7HKA) based custom board and we configure both SDHC interface.

SDHC1 is using for emmc support and SDHC2 is using for emmc too.

Emmc on the second eSDHC controller work normally.But Emmc on the first eSDHC controller does not work normally.

 

  1. SDHC1_CMD, SDHC1_CLK, SDHC1_DATA[3:0] are connected to the corresponding pins of eMMC; 


  1. SDHC1_CD_B is pulled up to O2VDD with a 10K resistor; SDHC1_WP is pulled down to GND through 1K resistance. SDHC1_VSEL is suspended (the development board is connected to the power chip MC34VR5100A1EP to control the voltage switch of SDHC1 interface power supply VCC_EVDD);


  1. SDHC1 interface power supply VCC_EVDD is always 1.8v.

 

It could not read and write to the eMMC after cold start, Through measuring the SDHC1 interface related pins in LS1012A with an oscilloscope, it was found that the waveform of the pin of eMMC was abnormal during the abnormal operation, and it could not drive to the low level state. The waveform of SDHC1_CLK pin is intercepted as follows:

pastedImage_1.png

But after power on for about 2.5 minutes, the eMMC worked normally. The emmc on the first eSDHC controller can read and write normally

 

Any pointers are greatly appreciated.

Have a great day,

       Diao

 

ラベル(2)
タグ(1)
0 件の賞賛
返信
12 返答(返信)

2,340件の閲覧回数
Hugh512
Contributor III

Set below configurations in RCW can solve the problem.
SDHC1_VSEL=0
EVDD_VSEL=1

0 件の賞賛
返信

3,007件の閲覧回数
haff
Contributor III

Hi Diao! Did the last suggestion to set SDHC1_VSEL and EVDD_VSEL to 0b00 help your problem? I am also interested in using SDHC1 for eMMC and I would really appreciate to if you'll share whether you've got it working in the end.

0 件の賞賛
返信

3,007件の閲覧回数
233158343
Contributor I


hi, ufedor


1. 62 pin (QSPI_A_SCK) is directly connected to QSPI NORFLASH without pull up and down.

2. 127 pin(SDHC2_CLK) is connected with eMMC mtfc64gakaeyf-4mit clock pin, which is pulled up to O1VDD through a 10K resistor;

3. 71 pin (SDHC1_CLK) is connected to eMMC mtfc64gakaeyf-4mit clock pin, and is pulled up to EVDD through a 10K resistor (in this design, EVDD = 1.8v, O1VDD, O2VDD and EVDD use the same power network)

4. 66 pin(SCAN_MODE_B) is pulled up to O1VDD through a 1K resistor.

I will be glad to any advice. Thank you.

0 件の賞賛
返信

3,007件の閲覧回数
ufedor
NXP Employee
NXP Employee

1) use a scope to ensure that the signal is not low during POR.

5) confirm that SDHC1_DAT[0:3] are pulled high through a 10-20 kΩ resistor to EVDD.

6) please provide U-Boot booting log as textual attachment

0 件の賞賛
返信

3,007件の閲覧回数
233158343
Contributor I

hi, ufedor

1.QSPI_A_SCK, SDHC2_CLK, SDHC1_CLK, SCAN_MODE_B are all high levels during the power-on reset.

2.SDHC1_DAT[0:3] was pulled to EVDD through a 20K pull-up resistor.

3.ESDHC1 is always 1.8v. Is there any problem with 1.8v during power on?
Note1:
“Though eSDHC1 boots at 3.3V, but it can dynamically switch to 1.8V controlled by the SDHC_VSEL signal.However, for eMMC 1.8V, the IO voltage can be set to 1.8V by default.”
Mentioned In QorIQ LS1012A Reference Manual.
Note1:
“eSDHC1: Supported primarily for SD cards. This is on the EVDD/O2VDD interface. CD/WP/VSEL are at 1.8V. Card initialization happens at 3.3V, but can dynamically switch to 1.8V controlled by the SDHC1_VSEL output pin. No provision to select EVDD=1.8V at boot time.”
Mentioned In AN5192 QorIQ LS1012A Design Checklist - Application Note.

4 Do the SDHC1_VSEL and EVDD_VSEL items in RCW need to be modified?


I will be glad to any advice. Thank you.

0 件の賞賛
返信

3,007件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please set SDHC1_VSEL and EVDD_VSEL to 0b00 instead of current 0b01.

0 件の賞賛
返信

3,007件の閲覧回数
233158343
Contributor I

hi, ufedor

 U-Boot booting log:


U-Boot 2016.092.0+ga06b209 (Mar 18 2019 - 19:58:17 -0700)

SoC: LS1012A Rev1.0 (0x87040110)
Clock Configuration:
CPU0(A53):1000 MHz
Bus: 250 MHz DDR: 1000 MT/s
Reset Configuration Word (RCW):
00000000: 0800000a 00000000 00000000 00000000
00000010: 35080000 c000000c 40000000 00001800
00000020: 00000000 00000000 00000000 00014571
00000030: 00000000 18c2a120 00000096 00000000
I2C: ready
DRAM: 510 MiB
SEC0: RNG instantiated
PPA Firmware: Version 0.2
Using SERDES1 Protocol: 13576 (0x3508)
MMC: before mmc_initializein mmc_initialize
before mmc_probe
in mmc_probe
uclass_foreach_dev device_probe
in fsl_esdhc_probe
fsl_esdhc_probe addr = 1560000
fsl_esdhc_probe bus_width = 1
fsl_esdhc_probe wp_enable = 0
fsl_esdhc_probe sdhc_clk = 125000000
in fsl_esdhc_init
in mmc_create
mmc_create success
fsl_esdhc_probe fsl_esdhc_init ok
uclass_foreach_dev device_probe
in fsl_esdhc_probe
fsl_esdhc_probe addr = 1580000
fsl_esdhc_probe bus_width = 1
fsl_esdhc_probe wp_enable = 0
fsl_esdhc_probe sdhc_clk = 125000000
in fsl_esdhc_init
in mmc_create
mmc_create success
fsl_esdhc_probe fsl_esdhc_init ok
FSL_SDHC: 0, FSL_SDHC: 1
SF: Detected S25FS512S with page size 256 Bytes, erase size 256 KiB, total 64 MiB
In: serial
Out: serial
Err: serial
Model: LS1012A RDB Board
Board: LS1012ARDB Error reading i2c boot information!
SATA link 0 timeout.
AHCI 0001.0301 32 slots 1 ports 6 Gbps 0x1 impl SATA mode
flags: 64bit ncq pm clo only pmp fbss pio slum part ccc apst
Found 0 device(s).
SCSI: Net: cbus_baseaddr: 0000000004000000, ddr_baseaddr: 0000000083800000, ddr_phys_baseaddr: 03800000
class init complete
tmu init complete
bmu1 init: done
bmu2 init: done
GPI1 init complete
GPI2 init complete
HGPI init complete
hif_tx_desc_init: Tx desc_base: 0000000083e40400, base_pa: 03e40400, desc_count: 64
hif_rx_desc_init: Rx desc base: 0000000083e40000, base_pa: 03e40000, desc_count: 64
HIF tx desc: base_va: 0000000083e40400, base_pa: 03e40400
HIF init complete
bmu1 enabled
bmu2 enabled
pfe_hw_init: done
pfe_firmware_init
pfe_load_elf: no of sections: 13
pfe_firmware_init: class firmware loaded
pfe_load_elf: no of sections: 10
pfe_firmware_init: tmu firmware loaded
PCIe0: pcie@3400000 Root Complex: no link
pfe_eth0, pfe_eth1
Hit any key to stop autoboot: 0
=>

0 件の賞賛
返信

3,007件の閲覧回数
ufedor
NXP Employee
NXP Employee

> The waveform of SDHC1_CLK pin is intercepted as follows:

?

> But after power on for about 2.5 minutes, the eMMC worked normally.

> The emmc on the first eSDHC controller can read and write normally

It is required to check POR levels and strapping of all signals having notes 5, 6, 8, 10 in the QorIQ LS1012A Data Sheet, Table 1. Pinout list by bus.

Ensure that TRST_B is pulsed low during the POR sequence.

0 件の賞賛
返信

3,007件の閲覧回数
233158343
Contributor I

hi, ufedor

According to your suggestion, we have made the following check

1 EMI1_MDCIIC1_SCL  and IIC1_SDA pin is not usedNo Connection

2 According to the datasheet, the rising edge of POR requires 8ns. Our board currently USES MAX6856UK16D3, and the rising edge time is about 50ns

3 The TRST_B is shorted to the PORESET_B to ensure that it is lowered during the power on.

4 EVDD power supply 1.8v directly

 

So my questions

Will the above differences lead to the current problems?

I would appreciate your advices!

Thanks, Diao

0 件の賞賛
返信

3,008件の閲覧回数
ufedor
NXP Employee
NXP Employee

What about pins:

62, 127, 71

66

0 件の賞賛
返信

3,008件の閲覧回数
233158343
Contributor I

hi, ufedor

    The waveform of SDHC1_CLK pin has been added to the above。

    SDHC2_CLK pin worked normally(1.8 v square wave).

Thank you,

Diao。

0 件の賞賛
返信

3,008件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please provide U-Boot booting log as textual attachment.

0 件の賞賛
返信