Hello!
In LSDK for LS1046ARDB the default configuration is including PPA in the QSPI flash image.
If I just do
CONFIG_FSL_LS_PPA=n
Is there anything else I should do instead to have a working LS1046A?
My backstory is that I just want to have highest access level all the time with access to all devices. The PPA code is dedicated to LS1046ARDB and since I'm running a custom LS1046A design I do not want to port it. I just want to remove it. Do I have to implement something else instead?
Thank you
BR
Robert
Use single image for u-boot and Linux.
NXP LSDK 18.09 provides u-boot binary image and Linux itb file for the LS1046ARDB board.
Find the "How to add support for a new custom machine in flexbuild based on LSDK release" in LSDK 1809 documentation.
Use the following commands for .itb file:
bootm a0000000#ls1046ardb
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------