I get the error:
Error with bitbake fsl-image-core for t2080rdb-64b: error: tclap-dev-1.2.1-r0 requires tclap = 1.2.1-r0
When I try: bitbake fsl-image-core
The log file has:
Computing transaction...warning: Can't install fmc-dev-git-r2@t2080rdb_64b: Can't install tclap-dev-1.2.1-r0@ppc64e6500: no package provides tclap = 1.2.1-r0
What do I need to do to fix this so I can complete the build?
thanks,
Kevin
Hello Kevin Dankwardt,
I am not sure which version Linux SDK you are using.
Please check whether the file meta-oe/meta-oe/recipes-devtools/tclap/tclap_1.2.1.bb exists in you workspace.
If not, please put the attached recipe file in the above path, and the source tar ball "git2_git.code.sf.net.p.tclap.code.tar.gz" in sources folder, and continue your current build.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------