Enabling the Ethernet Switch on LS1028ARDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enabling the Ethernet Switch on LS1028ARDB

580件の閲覧回数
sebastian_plama
Contributor II

I am trying to follow this documentation to enable the Switch on the LS1028ARDB:

https://docs.nxp.com/bundle/GUID-C3A436DA-E944-4F73-9811-2335DEBD04D6/page/GUID-558A9D18-5FA4-4E88-B...

All mentioned commands fail with the same error message:

 

 

 

root@localhost:~# restool dpsw create --num-ifs=5 --max-vlans=16 --max-fdbs=1 --options="DPSW_OPT_CTRL_IF_DIS"
error: Did not find a device file

 

 

 


The documentation also contains this line:

The following section describes the main commands to create a switch starting from the dpl-eth.0x2A_0x41.dtb DPL file.

Is there any description what this file is, where to find it, how to use it?

0 件の賞賛
2 返答(返信)

568件の閲覧回数
sebastian_plama
Contributor II

Thanks, I will try this.

Is there any way to know which parts of this very long document are relevant for which boards?

0 件の賞賛

574件の閲覧回数
bpe
NXP Employee
NXP Employee

restool and DPL files are valid only for devices equipped with DPAA2. LS1028A does not have it. Study this section of LSDK online documentation on how to work with LS1028A on-chip switch.

 

Hope this helps

Platon

 

0 件の賞賛