Does LS2084ardb only support 10gbase-kr for Backplane mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does LS2084ardb only support 10gbase-kr for Backplane mode

1,561 Views
howard12005
Contributor II

Hi,

I have a customized LS2084ARDB Board, 

I use Marvell switch 88E6191X 10G Port connect to Serdes1 10gbase-kr,

but there is a ping CPU port fail with the connection in uboot.

NXP FAE recommends that we refer to the AN12572 spec to set 10gbase-kr,

I would like to ask whether the support of 10Gbase-kr is only applicable to Backplane mode??

 

Is it necessary to set link_type = "MAC_LINK_TYPE_BACKPLANE" in dpc dts?

board_info {
ports {

mac@1 {
link_type = "MAC_LINK_TYPE_BACKPLANE";
             };
           …
             };
       };
};

Labels (1)
0 Kudos
Reply
4 Replies

1,436 Views
howard12005
Contributor II

Hi,Thanks Reply

I mean the location of mc_fw offset load,

like your link, It was supposed to be the first item load, but failed, so load the second item can also succeed,

1. QSPI location space

0x0000_2000_00000x0000_2FFF_FFFF256MBQuad SPI Region #1 (0-256MB)More QSPI space below 256MB

 

2. DRAM location space

0x0000_8000_00000x0000_9FFF_FFFF512MBGPP DRAM Region #1 (0-2GB)

 

Finally, dpmac is initialized successfully, and can ping mac IP in kerenl,
But always show this message: fsl-mc: Deploying data path layout ... WARNING: Firmware returned an error (GSR: 0x3f)

 

PCIe0: pcie@3400000 disabled
PCIe1: pcie@3500000 Root Complex: x4 gen3
PCIe2: pcie@3600000 Root Complex: no link
PCIe3: pcie@3700000 Root Complex: no link
DPMAC1@xgmii [PRIME]
SF: Detected mx25u6435f with page size 256 Bytes, erase size 64 KiB, total 8 MiB
device 0 offset 0x400000, size 0x300000
SF: 3145728 bytes @ 0x400000 Read: OK
device 0 offset 0x620000, size 0x100000
SF: 1048576 bytes @ 0x620000 Read: OK
crc32+
fsl-mc: Booting Management Complex ... SUCCESS
fsl-mc: Management Complex booted (version: 10.18.0, boot status: 0x1)
Hit any key to stop autoboot: 0
Switch 88E6191X all ports enable.
=> run bootcmd_nvme0

Device 0: Vendor: 0x1e95 Rev: 1.01 Prod: 0020341Y000K
Type: Hard Disk
Capacity: 122104.3 MB = 119.2 GB (250069680 x 512)
... is now current device
Scanning nvme 0:1...
Scanning nvme 0:2...
Found U-Boot script /ls2088ardb_boot.scr
961 bytes read in 0 ms
## Executing script at 80000000
22198280 bytes read in 25 ms (846.8 MiB/s)
32048 bytes read in 1 ms (30.6 MiB/s)
## Flattened Device Tree blob at 90000000
Booting using the fdt blob at 0x90000000
Loading Device Tree to 000000009fff5000, end 000000009ffffd2f ... OK
fsl-mc: Deploying data path layout ... WARNING: Firmware returned an error (GSR: 0x3f)

Starting kernel ...

0 Kudos
Reply

1,535 Views
howard12005
Contributor II

Hi,

Thanks, After initializing the marvell switch 10G serdes, can successfully ping to the cpu port
It means that the nxp cpu end to the marvell switch is connected in uboot

I will follow BACKPLANE mode to set the kernel dts, since serdes1 only uses 10gbase-kr pcs_mdio1,

1. then I need to disable emdio1 emdio2 in kernel dts?

2. I use QSPI flash to boot, and then mc, dpc, dpl firmware load dram space is successful, but load qspi space failed

    I refer to the LSDK code is default load qspi space, load dram space will this affect the dpaa2 ethernet connection?

 

&emdio1 {
    status = "disabled";
};

&emdio2 {
    status = "disabled";
};

&pcs_mdio1 {
        pcs_phy1ethernet-phy@0 {
        backplane-mode = "10gbase-kr";
        compatible = "ethernet-phy-ieee802.3-c45";
        reg = <0xa>;
        fsl,lane-handle = <&serdes1>;
        fsl,lane-reg = <0x9C0 0x40>;/* lane H */
    };
};
0 Kudos
Reply

1,462 Views
bpe
NXP Employee
NXP Employee

I'm not sure I understand your recent inputs. If you are having problems with
QSPI boot, please be sure to create a new thread or Support Case. I can only
tell that MC firmware, DPL and DPC binaries must be available at the addresses
specified in the corresponding arguments to fsl_mc u-Boot command when this
command is invoked. More details can be found in LSDK online documentation

https://docs.nxp.com/bundle/GUID-C3A436DA-E944-4F73-9811-2335DEBD04D6/page/GUID-81E61F39-077D-4384-9...

and u-Boot source code:

https://source.codeaurora.org/external/qoriq/qoriq-components/u-boot/tree/drivers/net/fsl-mc/mc.c

 

Best Regards,
Platon

 

0 Kudos
Reply

1,550 Views
bpe
NXP Employee
NXP Employee


Trust your FAE. Specifically for backplane-type connection and 10Gbps data rate,
10Gbase-KR is the only supported mode. Other 10Gbps SerDes modes require the
connected device to be a PHY or a device that behaves identically to a 10G PHY
and can be automatically recognized as such.

Section 2.2 of AN12572 clearly mentions that modifications to DPC are mandatory
for all DPAA2-based processors. LS2084 does belong to this category.

If the link does no work, the suggestions are:

  • Check with the documentation of device you connected that it does support 10GBase-KR
    and is properly configured for that.
  • Analyse the statistics at LS2084A side to have an idea of what is wrong.
    Follow AN12572 Section 4 to read the interface statistics information.

Hope this helps,
Platon

0 Kudos
Reply