I am using LSDK 17.09 for LS2088ARDB. I am trying to deploy a new rootfs on the device via tftp so I would like to rebuild the flex_linux_64.itb. Using the command in the flex-builder -i mkitb -a arm64 produce every time the same .itb altough I have installed new packages inside the rootfs.
Thanks,
Dorin
Use the following command:
mkimage -l image
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
And for the other question? If all I need to do is reconfigure RCW/PBI (i.e., I'm fine with the default firmware and kernel), is it safe to skip the .itb altogether, and reprogram just the RCW/PBI into bank 0?
Note: I've used the "Programming a New RCW" instructions in section 4.4.5.7 of the QorIQ SDK guide to verify that I can boot from bank 1 after programming my custom RCW/PBI. Does this mean it should be safe to program it into bank 0?
Look at the following page:
https://community.nxp.com/thread/448395
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Is there a way to inspect the contents of an .itb binary? In particular, I'm wondering what's contained in...
http://www.nxp.com/lgfiles/sdk/lsdk1709/flex_linux_arm64.itb
Some of the sample .its files I've seen in flexbuild include a ramdisk, but I haven't seen any specifying the actual ubuntu user land, and yet LSDK section 4.3 seems to imply that this one does. Am I misreading this section?
Also, does the alternate flash bank (bank 1, flash 2) contain the same default image as the primary bank when the LS1012A RDB ships? I don't really need to reprogram the image, but I need to program a custom RCW (and would prefer that it be in bank 0). Is it safe to reprogram just the RCW in bank 0? I mean, if I mess something up, is it possible to recover with CodeWarrior TAP?
Thanks,
Brett S.
Your are right. The simple help is available using the following command:
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Look at the Section 4.3 of LSDK documentation:
https://www.nxp.com/docs/en/supporting-information/LSDK-KC-REV0.pdf
Find the following:
locally build it using the command below:
$ flex-builder -i mkinstaller -a <arch> to generate flex_linux_<arch>.itb
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Pavel,
In LSDK 17.09 this command (mkinstaller) is not available maybe. I think it has been replaced by mkitb
~/workspace/LSDK/1709/flexbuild$ flex-builder -i mkinstaller -a arm64
INSTRUCTION: mkinstaller
DESTARCH: arm64
invalid instruction
Strange it is the LSDK documentation because in the flexbuild README is not present.
And as I said, mkitb build always same image with tiny distro.
Thanks,
Dorin
Thanks Pavel for you reply,
I have already done these steps and is working fine. What I asked is how could I regenerate the .itb to reflect my changes in rootf (so to get rid of the the tiny distro). For instance I need in rootfs : dpkg package but in this tinny distro it is not available. Everytime I generate .itb file same size is generated so does not reflect my local changes.
Thanks,
Dorin
Look at the Section 4.3 of LSDK documentation:
https://www.nxp.com/docs/en/supporting-information/LSDK-KC-REV0.pdf
For arm64 platforms:
=> tftp a0000000 flex_linux_arm64.itb
=> bootm a0000000#<board-name>
The <board-name> can be: ls1043ardb, ls1046ardb, ls1088ardb, ls2088ardb.
Command sequence for your configuration:
=> tftp a0000000 flex_linux_arm64.itb
=> bootm a0000000# ls2088ardb
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Pavel,
What format is the .itb file, and what exactly does it contain? My understanding is that an .itb is usually a combination "kernel + .dtb", but this one seems to contain the entire ubuntu user land as well. Is this so?
Also, what is the significance of address 0xa0000000? It seems to be a common load address, but I don't see it documented anywhere...
Finally, are the instructions in the referenced section valid for LS1012A? The referenced section says, "The <board-name> can be: ls1043ardb, ls1046ardb, ls1088ardb, ls2088ardb"
Thanks,
Brett S.