Hi,
I want to have clarification regarding Secure debug access Level 3 .
My doubt is:
If I just set(not permanently fuse) 0x100 in OEM Security Policy Register 1 (SFP_OSPR1) debug access level 3, what will be the effect on SDC?
Can I use SDC access level 3 in development (Lab) environment ?
Any help would be appreciated.
Thanks in advance,
Faizan
Hi Team,
Is there any update on above query ?
Regards,
Ashok
Hi
Just reminding for any suggestions..
Can we switch between levels on each power cycle in lab environment?
Any help or suggestions on this?
Hi @Faizanbaig
All the fuse are blown once bit. Once you burn a fuse bit from b'0 to a b'1, you cannot turn a fuse b'1 back to a b'0. That is why the
OEM Security Policy Register 1 (SFP_OSPR1), bit 29–31 DBLEV
000 Open: Debug portals are enabled unconditionally.
001 Conditionally closed via challenge response, without notification.
01x 01x: Conditionally closed via challenge response, with notification.
1xx 1xx: Closed. All debug portals are disabled.
instead of use decimal value 1,2,3,4.
Thanks
Khushbu