Compiling 88W9098 PCIe for LS1012A Dev Board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Compiling 88W9098 PCIe for LS1012A Dev Board

1,017件の閲覧回数
cdubs14
Contributor II

Hi,

I’m using the Type 1XL from Murata which uses the 88W9098 NXP chip and connects to the host via PCIe. I’ve plugged this board into a FRWY LS1012A development board running Layerscape. I’ve tried following the attached instructions from NXP for compiling the driver, but run into issues with the ‘make build’ command. I know I’m missing something with the Linux kernel but can’t figure out what, does anyone know how to resolve this to get the WiFi chip working?

タグ(3)
0 件の賞賛
返信
3 返答(返信)

800件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to "11.1 Connectivity for Bluetooth wireless technology and Wi-Fi" in i.MX_Linux_Users_Guide.pdf

0 件の賞賛
返信

884件の閲覧回数
kenli
NXP Employee
NXP Employee

question is not clear,u mean how to build the driver of 88w?

Best regards
0 件の賞賛
返信

870件の閲覧回数
cdubs14
Contributor II

Yep, just trying to compile the 88W9098 driver. I have the driver’s ‘make’ file, but I can’t figure out how to configure my Linux kernel to allow the ‘make build’ command execute successfully.

 

I’ve read online that I need to download and ‘setup’ the kernel, but I’m confused as to why that’s a step if I’m already running on the kernel version I’d like to use to building this driver. 

0 件の賞賛
返信