Hello,
We are currently designing LS1043A board. Does anyone know if the CodeWarrior for Networked Application support the LS1043A devices in the FC-PBGA (23x23 pkg. , FBGA780) package?
If so, how about the evaluation version? (It seems that there is no download shipment for the product version.)
Thanks in advance.
We are waiting for the arrival of the CodeWarrior and the hardware tools.
QCVS PinMuxing Tool (The evaluation version) cannot select the 23x23 package of LS1043A. Only 256pin is displayed.
How do I select the 23x23 package?
NXP offers CodeWarrior 11.5.0 for ARMv8:
This CodeWarrior supports the LS1043a in any package. This CodeWarrior uses CodeWarrior TAP hardware tool for connection via JTAG/COP interface to the LS1043a:
Use the CWH-CTP-CTX10-YE hardware tip for connection between CodeWarrior TAP and the LS1043a:
Evaluation version of this CodeWarrior provides full functionality for 15 days.