Closed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Closed

2,952 次查看
mrybaizine
Contributor II

Closed

0 项奖励
回复
6 回复数

2,709 次查看
yipingwang
NXP TechSupport
NXP TechSupport

This file is named rootfs_yocto_LS_arm64_tiny in LSDK 1909.

0 项奖励
回复

2,709 次查看
mrybaizine
Contributor II

Can you show responses for commands:

$ openssl version -a 

$ which openssl

$ uname -a

0 项奖励
回复

2,709 次查看
yipingwang
NXP TechSupport
NXP TechSupport

The above method doesn't work in LSDK 1909, you could add openssl in yocto:tiny manually.

$ flex-builder -c openssl -a arm64

$ sudo cp packages/apps/openssl/apps/openssl  build/rfs/rootfs_yocto_LS_arm64_tiny/target/usr/bin/

$ sudo cp packages/apps/openssl/lib*.so.*  build/rfs/rootfs_yocto_LS_arm64_tiny/target/lib/

$ flex-builder -i packrfs -r yocto:tiny -a arm64

0 项奖励
回复

2,709 次查看
mrybaizine
Contributor II

Did you try it ? or you misleading me again ?  First of all :

1.  $ flex-builder -c openssl -a arm64   will build ubuntu:main from scratch, not yocto ! 

Second and the most important 

Look at this:

mike-r@mike:~/work/flexbuild_lsdk1909$ flex-builder -c openssl -r yocto:tiny
COMPONENT: openssl
DISTRO TYPE: yocto
DISTRO SCALE: tiny
make: Entering directory '/home/mike-r/work/flexbuild_lsdk1909'
make[1]: Entering directory '/home/mike-r/work/flexbuild_lsdk1909/packages/apps'
make[1]: Leaving directory '/home/mike-r/work/flexbuild_lsdk1909/packages/apps'
make: Leaving directory '/home/mike-r/work/flexbuild_lsdk1909'
mike-r@mike:~/work/flexbuild_lsdk1909$

As you can see It is doing nothing because the Makefile  says don't do it for yocto:tiny !!!!
 

@[ $(DISTROTYPE) != ubuntu -a $(DISTROTYPE) != yocto -o $(DISTROSCALE) = mate -o $(DISTROSCALE) = lite -o $(DISTROSCALE) = tiny ] && exit || \
$(call fbprint_b,"OpenSSL") && $(call fetch-git-tree,openssl) && \

0 项奖励
回复

2,709 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please build openssl, then copy  binary and lib to build/rfs/rootfs_yocto_LS_arm64_tiny/target/, then generate yocto:tiny rootfs package.

0 项奖励
回复

2,709 次查看
mrybaizine
Contributor II

but you can't add openssl with lsdk1909  because  flex-builder lsdk1909 has bugs I pointed to in other threads. 

Why are you misleading me and the community? 

You say lsdk2004 will be released next month  in thread "NXP LSDK Has No Distro for production"

Also, the fact you copy a file somewhere doesn't mean everything works properly. At least, you have to show a response for command:

$ openssl version -a 

Why don't you give me lsdk2004 the way you gave me lsdk2003 with fixed linux boot error for  ubuntu:Lite ?

NXP didn't release lsdk_2003.  Maybe lsdk_2004 doesn't have to be released as well. 

0 项奖励
回复