Bring up Marvell 88E1543 on LX2160ARDB_REV2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bring up Marvell 88E1543 on LX2160ARDB_REV2

Jump to solution
4,116 Views
tsungmin_wang
Contributor III

Hi NXP,

We use SerDes 1 (0x7) and SerDes 2 (0xc).

There are two PHYs (Marvell 88E1543) connect to SGMII.

 

Here is my dts for SGMII

 

&dpmac7 {
	status = "okay";
	phy-handle = <&mdio2_phy1>;
	phy-connection-type = "sgmii";
};

&dpmac8 {
	status = "okay";
	phy-handle = <&mdio2_phy2>;
	phy-connection-type = "sgmii";
};

&dpmac9 {
	status = "okay";
	phy-handle = <&mdio2_phy3>;
	phy-connection-type = "sgmii";
};

&dpmac10 {
	status = "okay";
	phy-handle = <&mdio2_phy4>;
	phy-connection-type = "sgmii";
};

&dpmac11 {
	status = "okay";
	phy-handle = <&mdio2_phy5>;
	phy-connection-type = "sgmii";
};

&dpmac12 {
	status = "okay";
	phy-handle = <&mdio2_phy6>;
	phy-connection-type = "sgmii";
};

&dpmac17 {
	status = "okay";
	phy-handle = <&mdio2_phy7>;
	phy-connection-type = "sgmii";
};

&dpmac18 {
	status = "okay";
	phy-handle = <&mdio2_phy8>;
	phy-connection-type = "sgmii";
};

&emdio2 {
	status = "okay";
	mdio2_phy1: ethernet-phy@4 {
		reg = <0x4>;
	};
	mdio2_phy2: ethernet-phy@5 {
		reg = <0x5>;
	};
	mdio2_phy3: ethernet-phy@6 {
		reg = <0x6>;
	};
	mdio2_phy4: ethernet-phy@7 {
		reg = <0x7>;
	};

	mdio2_phy5: ethernet-phy@c {
		reg = <0xc>;
	};
	mdio2_phy6: ethernet-phy@d {
		reg = <0xd>;
	};
	mdio2_phy7: ethernet-phy@e {
		reg = <0xe>;
	};
	mdio2_phy8: ethernet-phy@f {
		reg = <0xf>;
	};
};

 

 

I enabled the driver for Marvell and added the support for 88E1543

 

static struct phy_driver M88E1543_driver = {
        .name = "Marvell 88E1543",
        .uid = 0x1410ea2,
        .mask = 0xffffff0,
        .features = PHY_GBIT_FEATURES,
        .config = &m88e151x_config,
        .startup = &m88e1011s_startup,
        .shutdown = &genphy_shutdown,
        .readext = &m88e1xxx_phy_extread,
        .writeext = &m88e1xxx_phy_extwrite,
};

 

 

I can get mdio info like this

 

=> mdio list
mdio@8b96000:
mdio@8b97000:
4 - Marvell 88E1543 <--> DPMAC7@sgmii
5 - Marvell 88E1543 <--> DPMAC8@sgmii
6 - Marvell 88E1543 <--> DPMAC9@sgmii
7 - Marvell 88E1543 <--> DPMAC10@sgmii
c - Marvell 88E1543 <--> DPMAC11@sgmii
d - Marvell 88E1543 <--> DPMAC12@sgmii
e - Marvell 88E1543 <--> DPMAC17@sgmii
f - Marvell 88E1543 <--> DPMAC18@sgmii

 

 

When I try to use one of them to ping, it occurred this error

 

Error: MC command failed (portal: 000000080c010000, obj handle: 0x27e, command: 0x1681, status: 0x7)
dprc_disconnect() failed dpmac_endpoint

 

 

 

0 Kudos
1 Solution
3,725 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the following suggestion from the expert team.

Suggest customer try to modify EC1_PMUX and EC2_PMUX with non-zero values in RCW in order to disable MAC17/18 RGMII mode.

View solution in original post

0 Kudos
12 Replies
4,106 Views
yipingwang
NXP TechSupport
NXP TechSupport

Your console log cannot be open, please attach it again if necessary.

Have you deployed MC and DPC firmware image on your target board?

Have you applied DPL file before booting up Linux Kernel?

Have you modified DPC and DPL files for your custom board?

In LSDK 21.08, you could run "$ flex-builder -c mc_utils", then get DPC and DPL source code in components/firmware/mc_utils/config/lx2160a/.

 

0 Kudos
4,102 Views
tsungmin_wang
Contributor III

Hi,

Yes, I have modified dpc and dpl for sgmii only.

I think it would apply dpl and dpc before kernel if using autoboot or "run bootcmd"

 

0 Kudos
4,071 Views
yipingwang
NXP TechSupport
NXP TechSupport

I have verified your dpl file on LX2160ARDB demo board.

I got similar booting up log as you.

[ 7.510687] fsl_dpaa2_eth dpni.11 (unnamed net_device) (uninitialized): PHY [0x0000000008b96000:02] driver [Qualcomm Atheros AR8035] (irq=POLL)
[ 7.524648] fsl_dpaa2_eth dpni.11: Probed interface eth1
[ 7.774684] fsl_dpaa2_eth dpni.10 (unnamed net_device) (uninitialized): PHY [0x0000000008b96000:01] driver [Qualcomm Atheros AR8035] (irq=POLL)

After under into Linux, I can ping server successfully through dpmac.17.

root@TinyLinux:~# ls-listni
dprc.1/dpni.11 (interface: eth1, end point: dpmac.18)
dprc.1/dpni.10 (interface: eth2, end point: dpmac.17)
dprc.1/dpni.9 (interface: eth3)
dprc.1/dpni.8 (interface: eth4)
dprc.1/dpni.7 (interface: eth5)
dprc.1/dpni.6 (interface: eth6)
dprc.1/dpni.5 (interface: eth7)
dprc.1/dpni.4 (interface: eth8)
dprc.1/dpni.3 (interface: eth9, end point: dpmac.6)
dprc.1/dpni.2 (interface: eth10, end point: dpmac.5)
dprc.1/dpni.1 (interface: eth11, end point: dpmac.4)
dprc.1/dpni.0 (interface: eth12, end point: dpmac.3)
root@TinyLinux:~# ifconfig eth2 100.1.1.100

root@TinyLinux:~# ping 100.1.1.1
PING 100.1.1.1 (100.1.1.1): 56 data bytes
64 bytes from 100.1.1.1: seq=0 ttl=64 time=0.509 ms
64 bytes from 100.1.1.1: seq=1 ttl=64 time=0.257 ms
64 bytes from 100.1.1.1: seq=2 ttl=64 time=0.234 ms
64 bytes from 100.1.1.1: seq=3 ttl=64 time=0.216 ms
64 bytes from 100.1.1.1: seq=4 ttl=64 time=0.261 ms

So, it seems that your dpl file can work, would you please try ping on your target board through dpmac.17.

If it failed, please try whether ping can work in u-boot through dpmac.17.

0 Kudos
4,067 Views
tsungmin_wang
Contributor III

I have tested in uboot and linux, both of them are failed.

u-boot,

=> ping 10.0.253.1
Error: MC command failed (portal: 000000080c010000, obj handle: 0x27e, command: 0x1671, status: 0x6)
dprc_connect() failed

 

linux,

Even through it can link up (only dpmac18@sgmii), but still can't ping out


Settings for eth0:
Supported ports: [ TP MII ]
Supported link modes: 10baseT/Full
100baseT/Full
1000baseT/Full
Supported pause frame use: Symmetric Receive-only
Supports auto-negotiation: Yes
Supported FEC modes: Not reported
Advertised link modes: 10baseT/Full
100baseT/Full
1000baseT/Full
Advertised pause frame use: Symmetric Receive-only
Advertised auto-negotiation: Yes
Advertised FEC modes: Not reported
Link partner advertised link modes: 10baseT/Half 10baseT/Full
100baseT/Half 100baseT/Full
1000baseT/Full
Link partner advertised pause frame use: Symmetric Receive-only
Link partner advertised auto-negotiation: Yes
Link partner advertised FEC modes: Not reported
Speed: 1000Mb/s
Duplex: Full
Port: Twisted Pair
PHYAD: 15
Transceiver: internal
Auto-negotiation: on
MDI-X: Unknown
Link detected: yes

root@localhost:~# ping 10.0.253.1
PING 10.0.253.1 (10.0.253.1) 56(84) bytes of data.
From 10.0.253.2 icmp_seq=1 Destination Host Unreachable
From 10.0.253.2 icmp_seq=2 Destination Host Unreachable
From 10.0.253.2 icmp_seq=3 Destination Host Unreachable
From 10.0.253.2 icmp_seq=4 Destination Host Unreachable
From 10.0.253.2 icmp_seq=5 Destination Host Unreachable
From 10.0.253.2 icmp_seq=6 Destination Host Unreachable

0 Kudos
4,035 Views
tsungmin_wang
Contributor III

Hi,

I have used the driver, but it doesn't solve the issue.

=> setenv ethact DPMAC7@sgmii
=> setenv ipaddr 10.0.253.2
=> ping 10.0.253.1
DPMAC7@sgmii Waiting for PHY auto negotiation to complete................................ TIMEOUT !
Using DPMAC7@sgmii

ARP Retry count exceeded; starting again
Error: MC command failed (portal: 000000080c010000, obj handle: 0x27e, command: 0x1681, status: 0x7)
dprc_disconnect() failed dpmac_endpoint
ping failed; host 10.0.253.1 is not alive
=> ping 10.0.253.1
DPMAC7@sgmii Waiting for PHY auto negotiation to complete................................ TIMEOUT !
Error: MC command failed (portal: 000000080c010000, obj handle: 0x27e, command: 0x1671, status: 0x6)
dprc_connect() failed

 

How can I solve the "MC command failed"?

Is something wrong with my dpc or dpl configuration?

0 Kudos
4,023 Views
yipingwang
NXP TechSupport
NXP TechSupport

Would you please try to ping  using DPMAC18@sgmii?

In addition, please read DPMAC18@sgmii PHY register to check the link status in u-boot.

=> mdio read DPMAC18@sgmii 1

I didn't find problem in your DPC and DPL file.

0 Kudos
3,958 Views
tsungmin_wang
Contributor III

 

=> mdio read DPMAC18@sgmii 1
Reading from bus mdio@8b97000
PHY at address f:
1 - 0x796d
=> mii dump 0xf 0x1
1.     (796d)                 -- PHY status register --
  (8000:0000) 1.15    =     0     100BASE-T4 able
  (4000:4000) 1.14    =     1     100BASE-X  full duplex able
  (2000:2000) 1.13    =     1     100BASE-X  half duplex able
  (1000:1000) 1.12    =     1     10 Mbps    full duplex able
  (0800:0800) 1.11    =     1     10 Mbps    half duplex able
  (0400:0000) 1.10    =     0     100BASE-T2 full duplex able
  (0200:0000) 1. 9    =     0     100BASE-T2 half duplex able
  (0100:0100) 1. 8    =     1     extended status
  (0080:0000) 1. 7    =     0     (reserved)
  (0040:0040) 1. 6    =     1     MF preamble suppression
  (0020:0020) 1. 5    =     1     A/N complete
  (0010:0000) 1. 4    =     0     remote fault
  (0008:0008) 1. 3    =     1     A/N able
  (0004:0004) 1. 2    =     1     link status
  (0002:0000) 1. 1    =     0     jabber detect
  (0001:0001) 1. 0    =     1     extended capabilities


=> ping 10.0.253.1
Error: MC command failed (portal: 000000080c010000, obj handle: 0x27e, command: 0x1671, status: 0x6)
dprc_connect() failed
ldpaa_dpmac_bind, DPMAC Type= dpmac
ldpaa_dpmac_bind, DPMAC ID= 3
ldpaa_dpmac_bind, DPMAC State= 0
ldpaa_dpmac_bind, DPNI Type=
ldpaa_dpmac_bind, DPNI ID= 0
ldpaa_dpmac_bind, DPNI State= -1
DPMAC link status: 1 - up
DPNI link status: 0 - down

Using DPMAC18@sgmii device

ARP Retry count exceeded; starting again
DPNI counters ..
DPNI_CNT_ING_ALL_FRAMES= 0
DPNI_CNT_ING_ALL_BYTES= 0
DPNI_CNT_ING_MCAST_FRAMES= 0
DPNI_CNT_ING_MCAST_BYTES= 0
DPNI_CNT_ING_BCAST_FRAMES= 0
DPNI_CNT_ING_BCAST_BYTES= 0
DPNI_CNT_EGR_ALL_FRAMES= 0
DPNI_CNT_EGR_ALL_BYTES= 0
DPNI_CNT_EGR_MCAST_FRAMES= 0
DPNI_CNT_EGR_MCAST_BYTES= 0
DPNI_CNT_EGR_BCAST_FRAMES= 0
DPNI_CNT_EGR_BCAST_BYTES= 0
DPNI_CNT_ING_FILTERED_FRAMES= 0
DPNI_CNT_ING_DISCARDED_FRAMES= 0
DPNI_CNT_ING_NOBUFFER_DISCARDS= 0
DPNI_CNT_EGR_DISCARDED_FRAMES= 0
DPNI_CNT_EGR_CNF_FRAMES= 0

DPMAC counters ..
DPMAC_CNT_ING_BYTE=15
DPMAC_CNT_ING_FRAME_DISCARD=9
DPMAC_CNT_ING_ALIGN_ERR =10
DPMAC_CNT_ING_BYTE=15
DPMAC_CNT_ING_ERR_FRAME=20
DPMAC_CNT_EGR_BYTE =21
DPMAC_CNT_EGR_ERR_FRAME =25
Error: MC command failed (portal: 000000080c010000, obj handle: 0x27e, command: 0x1681, status: 0x8)
dprc_disconnect() failed dpmac_endpoint
ping failed; host 10.0.253.1 is not alive

 

 

It looks like DPNI didn't work.

0 Kudos
3,938 Views
yipingwang
NXP TechSupport
NXP TechSupport

I need to discuss with the expert team.

0 Kudos
3,933 Views
tsungmin_wang
Contributor III

Hi,

Sorry, I found that I posted the wrong log for you.

The error code should be like this

 

ldpaa_dpmac_bind, DPMAC Type= dpmac
ldpaa_dpmac_bind, DPMAC ID= 17
ldpaa_dpmac_bind, DPMAC State= 0
ldpaa_dpmac_bind, DPNI Type= dpni
ldpaa_dpmac_bind, DPNI ID= 0
ldpaa_dpmac_bind, DPNI State= 0
DPMAC link status: 1 - up
DPNI link status: 1 - up
Using DPMAC17@sgmii device

ARP Retry count exceeded; starting again
DPNI counters ..
DPNI_CNT_ING_ALL_FRAMES= 0
DPNI_CNT_ING_ALL_BYTES= 0
DPNI_CNT_ING_MCAST_FRAMES= 0
DPNI_CNT_ING_MCAST_BYTES= 0
DPNI_CNT_ING_BCAST_FRAMES= 0
DPNI_CNT_ING_BCAST_BYTES= 0
DPNI_CNT_EGR_ALL_FRAMES= 0
DPNI_CNT_EGR_ALL_BYTES= 0
DPNI_CNT_EGR_MCAST_FRAMES= 0
DPNI_CNT_EGR_MCAST_BYTES= 0
DPNI_CNT_EGR_BCAST_FRAMES= 0
DPNI_CNT_EGR_BCAST_BYTES= 0
DPNI_CNT_ING_FILTERED_FRAMES= 0
DPNI_CNT_ING_DISCARDED_FRAMES= 0
DPNI_CNT_ING_NOBUFFER_DISCARDS= 0
DPNI_CNT_EGR_DISCARDED_FRAMES= 0
DPNI_CNT_EGR_CNF_FRAMES= 0

DPMAC counters ..
DPMAC_CNT_ING_BYTE=15
DPMAC_CNT_ING_FRAME_DISCARD=9
DPMAC_CNT_ING_ALIGN_ERR =10
DPMAC_CNT_ING_BYTE=15
DPMAC_CNT_ING_ERR_FRAME=20
DPMAC_CNT_EGR_BYTE =21
DPMAC_CNT_EGR_ERR_FRAME =25
Error: MC command failed (portal: 000000080c010000, obj handle: 0x27e, command: 0x1681, status: 0x7)
dprc_disconnect() failed dpmac_endpoint
ping failed; host 10.0.253.1 is not alive

 

 

We have two PHYs (88E1543) on our board. And the mode is SGMII-to-Copper (4 ports)

After testing, I found the there were two ports can ping success.

 

Serdes 1 with SGMII, all of the ports can't ping (DPMAC7~DPMAC10)

 

Serdes 2 with SGMII, two ports can ping and dhcp (DPMAC11, DPMAC12)

DPMAC17, DPMAC 18 would be failed.

 

Here is the ping success log

 

ldpaa_dpmac_bind, DPMAC Type= dpmac
ldpaa_dpmac_bind, DPMAC ID= 11
ldpaa_dpmac_bind, DPMAC State= 0
ldpaa_dpmac_bind, DPNI Type= dpni
ldpaa_dpmac_bind, DPNI ID= 0
ldpaa_dpmac_bind, DPNI State= 0
DPMAC link status: 1 - up
DPNI link status: 1 - up
Using DPMAC11@sgmii device
DPNI counters ..
DPNI_CNT_ING_ALL_FRAMES= 2
DPNI_CNT_ING_ALL_BYTES= 120
DPNI_CNT_ING_MCAST_FRAMES= 0
DPNI_CNT_ING_MCAST_BYTES= 0
DPNI_CNT_ING_BCAST_FRAMES= 0
DPNI_CNT_ING_BCAST_BYTES= 0
DPNI_CNT_EGR_ALL_FRAMES= 2
DPNI_CNT_EGR_ALL_BYTES= 84
DPNI_CNT_EGR_MCAST_FRAMES= 0
DPNI_CNT_EGR_MCAST_BYTES= 0
DPNI_CNT_EGR_BCAST_FRAMES= 1
DPNI_CNT_EGR_BCAST_BYTES= 42
DPNI_CNT_ING_FILTERED_FRAMES= 0
DPNI_CNT_ING_DISCARDED_FRAMES= 0
DPNI_CNT_ING_NOBUFFER_DISCARDS= 0
DPNI_CNT_EGR_DISCARDED_FRAMES= 0
DPNI_CNT_EGR_CNF_FRAMES= 0

DPMAC counters ..
DPMAC_CNT_ING_BYTE=15
DPMAC_CNT_ING_FRAME_DISCARD=11
DPMAC_CNT_ING_ALIGN_ERR =10
DPMAC_CNT_ING_BYTE=15
DPMAC_CNT_ING_ERR_FRAME=22
DPMAC_CNT_EGR_BYTE =23
DPMAC_CNT_EGR_ERR_FRAME =27
host 10.0.253.1 is alive

 

 

0 Kudos
3,726 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the following suggestion from the expert team.

Suggest customer try to modify EC1_PMUX and EC2_PMUX with non-zero values in RCW in order to disable MAC17/18 RGMII mode.

0 Kudos
3,722 Views
tsungmin_wang
Contributor III

Hi,

This is solved, thanks.

And I have known the critical issue.

tsungmin_wang_0-1642400894892.png

This is the setting we use, but unfortunately, the PLL mapping is not match.

Our PLLF is 156.25 MHz and PLLS is 100 MHz.

XFI (the other issue) and USXGMII should use PLLF, and SGMII should use PLLS.

But the mapping is just reversed. I just tested this setting which SGMII interfaces use PLLS.

tsungmin_wang_1-1642401055190.png

And the PHY on Serdes 1 ping to network successfully in uboot.

 

So, I wonder how to configure the PLL mapping of the option 7 to FFFFSSSS. thanks.

0 Kudos