Hello all,
We've got a new LS1043 based SBC and it's generally working well. We can get to the U-Boot prompt, boot Linux, etc. But in order to do this, we had to remove most of the functions in arch_cpu_init(). Specifically, we have to remove __asm_invalidate_dcache_all(), __asm_invalidate_tlb_all(), and early_mmu_setup(). This is our first ARM card, so I'm still getting up to speed on ARM, but I can't figure out why these things would cause the board to hang. We don't have an ARM JTAG debugger, so I haven't been able to look at exactly what's going wrong. Anyone got any suggestions?
Thanks,
John
Hello Fedor,
Sorry for the delay. The pre-built images wouldn't work on any board other than your development system because of your QIXIS FPGA. I downloaded the 2.0 SDK and I had to take quite a bit out of the LS1043AQDS image, but I tested with and without those lines I mentioned and it boots without and doesn't with.
I did notice one very interesting thing. We were able to get the QSPI image working. This QSPI QDS image does not include arch_cpu_init(). The SPL image only includes arch_cpu_init() if the board is an LS2080A. Could this just be an oversight for NOR boot? Perhaps arch_cpu_init() should not be called for the LS1043A?
Thanks,
John
We have an RDB, but we cannot run the precompiled binaries on our hardware. The precompiled binary does run on the RDB. But SDK 2.0 also does not call arch_cpu_init(). That call was introduced in mainline when ARM moved to the unified arch/arm/lib/board.c. It seems like that function is the weak link, it's not meant to be called on the LS1043A. Can you confirm that this needs to be changed in mainline U-Boot?
> We have an RDB, but we cannot run the precompiled binaries on our hardware.
> The precompiled binary does run on the RDB.
This means that you have to doublecheck your design referring the AN5012 - LS1043A Design Checklist and the processor's Data Sheet (pay special attention to the notes after Table 1 and Table 2).