Board version of LS1021A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Board version of LS1021A

Jump to solution
887 Views
pengcheng
Contributor III

I have three boards labeled with 700-28040 REV C , 700-28040 REV X4 and 700-28973 REV A.

Are the first two the same type boards named LS1021ATWR?

Is the last one the board named LS1021ATWR-PB?

Thanks!

Labels (1)
Tags (1)
1 Solution
768 Views
alexander_yakov
NXP Employee
NXP Employee

Yes, 700-28040 means TWR-LS1021A board.

For 700-28973 - this number is incorrect, I assume you meant 700-28673, this is correct number for TWR-LS1021A-PB.  


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
769 Views
alexander_yakov
NXP Employee
NXP Employee

Yes, 700-28040 means TWR-LS1021A board.

For 700-28973 - this number is incorrect, I assume you meant 700-28673, this is correct number for TWR-LS1021A-PB.  


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

768 Views
pengcheng
Contributor III

Yes, you are right, Thank you!

0 Kudos