DDR3L bit swapping with LS1012A processor within byte

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR3L bit swapping with LS1012A processor within byte

2,172 Views
nilavchoksi
Contributor III

Hello,

I am designing custom board using LS1012A processor and interface with two 1Gx8 DDR3L micron DDR3L chip.

During layout, I am facing issue of routing of data lines so that as per AN3940 (Hardware and Layout Design
Considerations for DDR3 SDRAM Memory Interfaces) I have swapped the datalines in D0 to D7 at first DDR3L end.

Also, attached swapped connections of first DDR3L with Processor.

So, will it work for me? because I can't see any information or guide to change this bits from firmware configuration level and confusion on the connections.

Looking for your help.

Labels (1)
1 Reply

1,942 Views
ufedor
NXP Employee
NXP Employee

It is possible to swap bits within a byte lane.

Please refer to the AN3940, Table 1. DDR3 Designer Checklist, 45:

https://www.nxp.com/webapp/Download?colCode=AN3940

Note that the MMDC supports only x16 data bus width.

0 Kudos
Reply