Audio Video bridge for LS1021A-IOT

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Audio Video bridge for LS1021A-IOT

1,669 次查看
prabinca4u
Contributor III

Hi dear freescale team

Right now I'm working on LS1021A-IOT to implement AVB on that. I have an Open AVB but it is for NIC CARD (using PCI), I want to test AVB without NIC CARD ie direclty use eth0 or eth1 interface on LS1021A-IOT board. So I need the AVB source code for this, Can you please provide me the link for download freescale generic AVB source code.

标签 (1)
3 回复数

1,265 次查看
Pavel
NXP Employee
NXP Employee

Look at the following pages about inspection of gsteamer:

https://gstreamer.freedesktop.org/data/doc/gstreamer/head/faq/html/chapter-using.html

https://gstreamer.freedesktop.org/data/doc/gstreamer/head/manual/html/section-checklist-applications...

http://docs.gstreamer.com/display/GstSDK/gst-inspect


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,265 次查看
Pavel
NXP Employee
NXP Employee

Look at the following page:

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/s32-processors-and-microc...

Find "Supporting device" on this page.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,265 次查看
prabinca4u
Contributor III

Thanks pavel for your reply

I got an open AVB, And I just cross compiled it for my LS1021A-IOT. My aim is to test talker listener program on two separate LS1 board respectively. On taker it use gstreamer-1.0 for sending  the simple sine audio to listener by entering given command at talker as shown below .

gst-launch-1.0 -v -e alsasrc device=hw:0,0 do-timestamp=true ! audioconvert ! audioresample ! wavenc ! fdsink | ./talker eth0 256

when I run this I got error like this "WARNING: erroneous pipeline: no element wavenc""

And is listener side

./listener eth0 256 | gst-launch-1.0 fdsrc fd=0 ! audioparse rate=32000 channels=2 ! alsasink sync=false async=false

On running this I'm getting error like "WARNING: erroneous pipeline: no element audioparse".

I have Installed gstreamer-1.0 and plugins (good,bad,ugly,base,meta-base and omx). Even though the audioparse functionality at listener and wavenc at talker is not getting for gstreamer.

But gstreamer-1.0 have the plugins such as  alsasrc, audioconvert, audioresample, fdsink, alsasink. That I have verified with gst-inspect command.

But on verifying this for wavenc and audioparse , I got "No such element or plugin 'waveenc OR audioparse' "

0 项奖励
回复