我要适配一个ls1043板子我该如何操作?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

我要适配一个ls1043板子我该如何操作?

跳至解决方案
873 次查看
小狼
Contributor I

我有一块板子ls1043a,如果需要适配这块板子,我需要做什么?,需要更新uboot吗?

那要如何操作?有适配案例吗,如果更新uboot失败会不会导致ttl无法进入,只能用编程器?

 


U-Boot 2018.09.HX.002-00013-g59e353dea8 (Nov 11 2020 - 17:48:01 +0800)

Clock Configuration:
CPU0(A53):1600 MHz CPU1(A53):1600 MHz CPU2(A53):1600 MHz
CPU3(A53):1600 MHz
Bus: 400 MHz DDR: 1600 MT/s FMAN: 500 MHz
Reset Configuration Word (RCW):
00000000: 08100010 0a000000 00000000 00000000
00000010: 45580002 80004012 40044000 c1002000
00000020: 00000000 00000000 00000000 0002cffd
00000030: 20004500 001e3208 00000096 00000001
Model: LS1043A NH03 Board
Board: NH03 V100, boot from QSPI
DRAM: 1.9 GiB (DDR4, 32-bit, CL=11, ECC off)
Using SERDES1 Protocol: 17752 (0x4558)
Loading Environment from SPI Flash... OK
Net: Fman1: Uploading microcode version 106.4.18
PCIe0: pcie@3400000 Root Complex: no link
PCIe1: pcie@3500000 Root Complex: x1 gen1
PCIe2: pcie@3600000 disabled
FM1@DTSEC1, FM1@DTSEC2, FM1@DTSEC3 [PRIME], FM1@DTSEC4, FM1@DTSEC5, FM1@DTSEC6
Temp:
01_4c local 48 C
01_4c remote 58 C
MMC:
FSL_SDHC: 14.6 GiB
SPI FLASH:
8 MiB

0 项奖励
回复
1 解答
850 次查看
June_Lu
NXP TechSupport
NXP TechSupport

If the board in your hand is LS1043ARDB Layerscape LS1043A Reference Design Board | NXP Semiconductors, you could refer the guide below.  If not, you could refer the LS1043ARDB.

The guide please refer to LSDK21.08, page 97, 4.1.9 LSDK Quick Start Guide for LS1043ARDB or Layerscape Linux Distribution POC User Guide, Rev. L6.1.1-1.0.0 page 46, 4.7.5 Quick start guide for LS1043ARDB.

It depends which SW version you choose.

The RDB has user selectable switches for evaluating different boot options for the LS1043A device, NOR, NAND, SD. When one boot mode fail to boot up, you could choose another one. You could find the boot mode information from the Chapter I shared above.

To keep the board boot up successfully, it will be better to make sure all boot modes work well, you could follow the guide to download the default image and program them, especially the SD mode, maybe you can prepare more than one card.

If all the boot modes are corrupted in the image update, you have to use the CW to program the board.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
851 次查看
June_Lu
NXP TechSupport
NXP TechSupport

If the board in your hand is LS1043ARDB Layerscape LS1043A Reference Design Board | NXP Semiconductors, you could refer the guide below.  If not, you could refer the LS1043ARDB.

The guide please refer to LSDK21.08, page 97, 4.1.9 LSDK Quick Start Guide for LS1043ARDB or Layerscape Linux Distribution POC User Guide, Rev. L6.1.1-1.0.0 page 46, 4.7.5 Quick start guide for LS1043ARDB.

It depends which SW version you choose.

The RDB has user selectable switches for evaluating different boot options for the LS1043A device, NOR, NAND, SD. When one boot mode fail to boot up, you could choose another one. You could find the boot mode information from the Chapter I shared above.

To keep the board boot up successfully, it will be better to make sure all boot modes work well, you could follow the guide to download the default image and program them, especially the SD mode, maybe you can prepare more than one card.

If all the boot modes are corrupted in the image update, you have to use the CW to program the board.

0 项奖励
回复
841 次查看
小狼
Contributor I
什么是CW?
0 项奖励
回复