no emulator/ board detected

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

no emulator/ board detected

537件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheAlex on Tue Jul 31 09:39:58 MST 2012
Hello,
I am trying to run the default project blinky and getting the following error.
[IMG]http://i50.tinypic.com/2v1xk03.png[/IMG]

the run menu also seems to be limited.
[IMG]http://i50.tinypic.com/2i23n2u.png[/IMG]

I am able to debug the same code using keil c but no luck with lpc xpresso.

Any help highly appreciated.
thanks in advance.
Alex.
0 件の賞賛
返信
7 返答(返信)

527件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheAlex on Wed Aug 22 12:01:31 MST 2012
Thank you all for the kind and valuable response!! Right now I have access to LPC link. At the time of debugging the usb device is getting disconnected. I just made a video on the problem I'm facing right now. Please refer http://youtu.be/EmDSbFmA8BQ?hd=1

thanks in advance.
Alex.
0 件の賞賛
返信

527件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Wed Aug 01 00:25:13 MST 2012
ulink-me is not supported by LPCXpresso.
LPCXpresso supports LPC-Link and Red Probe+
0 件の賞賛
返信

527件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cylim on Tue Jul 31 23:10:48 MST 2012
No emulator and error lauching debug! any useful solution?
0 件の賞賛
返信

527件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheAlex on Tue Jul 31 14:53:58 MST 2012
**I'm using uLink-me http://www.keil.com/ulinkme/
Is it compatible with LPC xpresso ?
Thanks



Quote: TheFallGuy
Are you *sure* you are using LPC-Link? AFAIK, Keil do not support it, so I don't think you can be using LPC-Link.

0 件の賞賛
返信

527件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Tue Jul 31 14:28:00 MST 2012
Are you *sure* you are using LPC-Link? AFAIK, Keil do not support it, so I don't think you can be using LPC-Link.
0 件の賞賛
返信

527件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheAlex on Tue Jul 31 14:12:32 MST 2012
Hello,
Thank you for the response.
I am using NXP lpc link and 10 pin cable to connect the LPC4330 board. With the same setup I am able to debug using keil C.



Quote: TheFallGuy
How have you connected LPC-Link? You will need to split it and use the 10-pin connector to connect to your targets JTAG/SWD connector

0 件の賞賛
返信

527件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Tue Jul 31 10:04:55 MST 2012
How have you connected LPC-Link? You will need to split it and use the 10-pin connector to connect to your targets JTAG/SWD connector
0 件の賞賛
返信