flash more than 256k on lpc1788 without unlimited license

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

flash more than 256k on lpc1788 without unlimited license

484件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Gonzalo_Sipel on Thu Jan 07 07:50:20 MST 2016
Hi everyone:
We have developed a custom board based on LPC1788 and we have written a firmware which is 450 kbytes long. Here in the engineering office we have our lpcxpresso with unlimited license but we need upload code in production sector and there is non unlimited license. Is there any way to upload code using LPC-Link without an unlimited license? (We don´t want debug code, just upload the code).

thanks!
0 件の賞賛
8 返答(返信)

439件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Gonzalo_Sipel on Fri Jan 08 07:29:56 MST 2016
Thanks R2D2!
0 件の賞賛

439件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Fri Jan 08 07:16:31 MST 2016

Quote: Gonzalo_Sipel
Does anyone know something about this?



Just create a hex file and use Interface: SWD over Link2. No restrictions...
0 件の賞賛

439件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Gonzalo_Sipel on Fri Jan 08 06:22:11 MST 2016
vtw.433e
I've been looking for information about LPC-Link2 and what you have suggested seems to be the best option. Have you used flashMagic with LPC-Link2? Do you know if there is any restriction about code size?  Does anyone know something about this?
Regards!
0 件の賞賛

439件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vtw.433e on Thu Jan 07 13:23:37 MST 2016
Well buy an Lpc-link2 then. They are about $15. You've probably wasted several times that already!
0 件の賞賛

439件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Gonzalo_Sipel on Thu Jan 07 11:39:16 MST 2016
vtw.433e, I am trying to use a lpc-link debugger which is not the same that lpc-link2 debugger
0 件の賞賛

439件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vtw.433e on Thu Jan 07 09:03:12 MST 2016
According to the FlashMagic release notes, it does support programming using LPC-Link2:

Quote:
v9.30
- Added support for standalone LPC-Link2 for USB to SWD programming.




However, to use Flash Magic in a production environment, you have to purchase a license...
0 件の賞賛

439件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Gonzalo_Sipel on Thu Jan 07 08:08:24 MST 2016
Mysepp:
We are able to use flashMagic but it is too slow, it takes about 8 minutes each load.
0 件の賞賛

439件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mysepp on Thu Jan 07 07:54:36 MST 2016
Must it be over LPC-Link or is perhaps uploading via ISP/serial port (via USB) a solution?
Look for FlashMagic.
0 件の賞賛