Hi to all
I've bought two LPClink2 boards but I can't debug a board with LPC114 using them. When I start to debug
with LPCXpresso (8.2.2) in first a windows notify me that:
Initializing link server with LPC432x_CMSIS_DAP_V5_173.bin.hdr
after some time, the result is :
Timeout waiting LinkServer to initialize(0)
and if I abort and see log error message, the end of message is :
finished! Resetting USB to switch back to runtime mode
That is seems that it download correctly the firmware and can't reset the board. Anyone experienced this ?
How can I solve ?
Regards
That sounds like the mouse transmitter is also using DFU boot to download firmware, and that there is some strange clash.
You might want to consider programming the Link2 firmware into flash directly to avoid this (rather than having the IDE softload at first connect time). You can do this using the LPCScrypt utility. For more details, please see:
https://community.nxp.com/message/630661
Regards,
LPCXpresso Support
Hello everybody. I had the very same problem right now. OS is windows 10, LPC-Link 2 enumerates but linkserver doesn't start with similar error message. I've made it work somehow. Strangely enough, there was some kind of conflict with the transmitter of wireless mouse. So, the sequence of actions in my case was the following:
1. Unplug the mouse transmitter.
2. Execute "C:\nxp\LPCXpresso_8.2.2_650\lpcxpresso\bin>boot_link2". It replies with "LPC-Link2 booted" message.
3. Plug the mouse transmitter back.
Now LPCXPresso works normally with the debugger.
Please run through the manual booting process described in the FAQ that we point you at previously, and if you are still having problems then tell us what you see at each of FAQ steps. You should also check out the Troubleshooting section at the end.
https://community.nxp.com/message/630577
Also, what OS are you using?
Regards,
LPCXpresso Support
I would also suggest taking a look at this FAQ, in particular the troubleshooting section:
https://community.nxp.com/message/630577
Regards,
LPCXpresso Support
First, I presume you meant to type LPC1114, but you didn't include any host related details. Is there anything in the debug log you can post?
Thanks and regards,
LPCXpresso Support