Problem flushing LPCXpresso LPC1769 (Rev. B 2010) with lpcexpresso 8.2.2 & MacOS Maveriks (10.9.5)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem flushing LPCXpresso LPC1769 (Rev. B 2010) with lpcexpresso 8.2.2 & MacOS Maveriks (10.9.5)

547件の閲覧回数
stanislavsilnic
Contributor I

Hello,

I've installed and activated lpcexpresso 8.2.2 in my macbook. Then, trying to flush blink example, I've got an error.

Screenshot at Apr 24 05-42-09.png

This error has appeared as well when I tried to boot manually:

bash-3.2$ ./dfu-util -d 0x471:0xdf55 -c 0 -t 2048 -R -D LPCXpressoWIN.enc

dfu-util 0.9

Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc.

Copyright 2010-2016 Tormod Volden and Stefan Schmidt

This program is Free Software and has ABSOLUTELY NO WARRANTY

Please report bugs to http://sourceforge.net/p/dfu-util/tickets/

dfu-util: Invalid DFU suffix signature

dfu-util: A valid DFU suffix will be required in a future dfu-util release!!!

dyld: lazy symbol binding failed: Symbol not found: _OSAtomicIncrement32Barrier

  Referenced from: /Applications/lpcxpresso_8.2.2_650/lpcxpresso/bin/./libusb-1.0.0.dylib

  Expected in: /usr/lib/libSystem.B.dylib

dyld: Symbol not found: _OSAtomicIncrement32Barrier

  Referenced from: /Applications/lpcxpresso_8.2.2_650/lpcxpresso/bin/./libusb-1.0.0.dylib

  Expected in: /usr/lib/libSystem.B.dylib

Trace/BPT trap: 5

bash-3.2$

Is it possible to continue working with LPCExpresso board in my environment?

Stan

ラベル(2)
0 件の賞賛
2 返答(返信)

276件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

On further investigation we can see that you have identified a compatibility issue between LPCXpresso IDE 8.2.2 and Mac OSX 10.9.5.

Unfortunately the options available are to downgrade your version of LPCXpresso IDE to version 7.9, or to upgrade the version of OSX running on your Mac.

Yours,

LPCXpresso Support

0 件の賞賛

276件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

Initially I suggest you take a look at the following FAQ https://community.nxp.com/message/630541 this provides some background and a trouble shooting section.

Yours

LPCXpresso Support

0 件の賞賛