Content originally posted in LPCWare by Kaveh.t on Tue Mar 03 19:13:38 MST 2015
Hi there,
There are some changes i generated,
1) I changed my Workspace and deleted all The LPC open Libarys and Examples
2) Imported the CMSIS _Core_LPC11 Libary in my Workspace
3 ) From the LPC_Xpresso_11xx Examples ( Not anymore LPC_Open), i inserted the Blinky Example File into Workspace.
4 ) The main c File named blinky.c has a source code, This source code i deleted and write my own source code to it, which is for my PCB Projekt that i construkted.
5) Then I linked bouth the Libary Paths, and the header Include Files from the CMSIS_Core_LPC11xx to the Blinky Projekt. This Procedure for Debug and same for Release
6 ) on my PCB i have implemented LPC1112/ 201 µC and connected it to a LED.
7 ) when I Debug there are further 10 Error Messages
Console Code :
ake: *** [src/blinky.o] Error 1
02:49:35 Build Finished (took 170ms)
Files are added as Attachement
Has anyone the capability to make this File compatible, to solve this issue and that i can write my LED Source Code in the Blinky.c File and Compile it without getting error messages, thats just a LED Programm.
Kindly Regards
Kaveh
ake: *** [src/blinky.o] Error 1
02:49:35 Build Finished (took 170ms)