$ java -version java version "1.7.0_51" Java(TM) SE Runtime Environment (build 1.7.0_51-b13) Java HotSpot(TM) 64-Bit Server VM (build 24.51-b03, mixed mode) |
$ ./lpcxpresso_6.1.4_194/lpcxpresso/lpcxpresso Gtk-Message: Failed to load module "canberra-gtk-module" (lpcxpresso:7868): Gtk-WARNING **: Unable to locate theme engine in module_path: "oxygen-gtk", (lpcxpresso:7868): Gtk-WARNING **: Unable to locate theme engine in module_path: "oxygen-gtk", (process:7912): GLib-CRITICAL **: g_slice_set_config: assertion 'sys_page_size == 0' failed # # A fatal error has been detected by the Java Runtime Environment: # # SIGSEGV (0xb) at pc=0xc38c623e, pid=7868, tid=4149212928 # # JRE version: 7.0_25-b30 # Java VM: OpenJDK Client VM (23.7-b01 mixed mode linux-x86 ) # Problematic frame: # C [libgobject-2.0.so.0+0x1723e] g_object_get_qdata+0x1e # # Failed to write core dump. Core dumps have been disabled. To enable core dumping, try "ulimit -c unlimited" before starting Java again # # An error report file with more information is saved as: # /home/renan/hs_err_pid7868.log # # If you would like to submit a bug report, please include # instructions on how to reproduce the bug and visit: # https://bugs.launchpad.net/ubuntu/+source/openjdk-7/ # The crash happened outside the Java Virtual Machine in native code. # See problematic frame for where to report the bug. # Aborted (core dumped) |
Original Attachment has been moved to: hs_err_pid7868.txt.zip
$ pwd /home/renan/lpcxpresso_6.1.4_194/lpcxpresso/jre/bin [renan@arch64 bin]$ ./java -version java version "1.7.0_25" OpenJDK Runtime Environment (IcedTea 2.3.10) (7u25-2.3.10-1ubuntu0.12.04.2) OpenJDK Server VM (build 23.7-b01, mixed mode) |
-vm jre/bin/java |