LPCXpresso 5.2.2 released

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCXpresso 5.2.2 released

160 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu Apr 18 02:47:50 MST 2013
LPCXpresso v5.2.2 has been released. Changes include

* Upgrade all Eclipse components to latest Juno SR2 release
* Made breaks in instruction trace more visible.
* Added indication of unapplied changes in instruction trace settings.
* Disabled configuration of unsupported Auto-halt functionality for LPC800.
* Fixed linker issue related to load address of initialized data items aligned to >4 byte boundaries
* Improved display of registers after a Fault on Cortex-M cores
* Fixed issue with flash programming utility for image paths containing spaces
* Fix update of Quickstart buttons if active build configuration is changed
* Fix display of mixed source in Disassembly View
* Add preference to display (hex) opcodes in Disassembly View
* Added 'Attach only' option to debug configuration to attach to a running processor
* Much improved project support for Multicore processors (such as LPC43xx)
* Updated LPC43xx Peripheral Driver Library port.
* Added flash driver support for Diolan LPC1850-DB1 / LPC4350-DB1 boards
* Additional examples for LPC43xx boards
* Standardised flash programming for LPC11/12/13/17; Same mechanism used with all probes.
* NXP LPC800 project wizards updated to support MTB setup
0 Kudos
Reply
0 Replies