LPCXpresso 1769 Reset behaviour

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCXpresso 1769 Reset behaviour

190 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by boater on Tue Jul 09 05:37:09 MST 2013
Hello

I have a weird issue with a LPCXpresso 1769 board, mounted on a protoboard. In case the 1769 is powered over the 3.3V pin only, it seems that LPCLink part gets powered as well, causing the Reset line to go low. Interestingly, power goes away e.g. when I put the cap on the JTAG pins and remove it, so perhaps something gets charged and is discharged by those kind of actions. Is the circuit so sensitive? Is there any advise on how to deal with this?

Thanks,
Peter
0 项奖励
回复
0 回复数