Jtag connection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Jtag connection

565 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by unnati on Mon Mar 08 23:26:33 MST 2010
hi,

plz tell me the connections of JTAG pins to be connected to the LPC1114.

i can download the program in the target provided in the LPCkit.

but m not able to download the same program in my own target board...it shows error in connection.so let me know the pin connections of JTAG.

i am stuck
0 Kudos
4 Replies

533 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Europe on Wed Mar 10 01:17:03 MST 2010
Hi unnati,
Got it working?

Cheers,
0 Kudos

533 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by unnati on Wed Mar 10 00:38:24 MST 2010
thanx both of u..:)
0 Kudos

533 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Europe on Tue Mar 09 07:16:33 MST 2010
Hi unnati,

Please note that the LPC1300 and LPC1100 doesn't have JTAG but SWD only. This is probably not you problem, but is worth while to mention.

Indeed Fig 34 of the getting started guide shows which connections are needed for SWD. Not all pins are needed for the LPC1114, only the  SWDIO, SWCLK, RESET and GND are recommended to connect.

Kind regards,
0 Kudos

533 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wrighflyer on Tue Mar 09 04:03:57 MST 2010

Quote: unnati
hi,

plz tell me the connections of JTAG pins to be connected to the LPC1114.

i can download the program in the target provided in the LPCkit.

but m not able to download the same program in my own target board...it shows error in connection.so let me know the pin connections of JTAG.

i am stuck


The pinout of the JTAG header on the LPC-Link is given in the "Getting started" PDF guide
0 Kudos