How to share PLU schematic between projects

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to share PLU schematic between projects

2,584 Views
_Ferrari_
Contributor V

Dear all,

Im using MCUXpresso IDE v11.7.0 [Build 9198] [2023-01-17] and I developed a project, based on LPC5526 cpu, in which I used schematic tool to design PLU logic.

Now I want to reuse the same schematic and the same logic in another project based on LPC55xx processor family.

Is it possible to 'export' only the schematic and 'import' it in another project ?

thank you very much for your help and cooperation

regards

 

0 Kudos
Reply
3 Replies

2,558 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @_Ferrari_ 

 

The project based on MCUXpresso IDE use the generate code from schematic, not use the schematic file, so you just need copy and paste code into your new project as XiangJun Rong said.

 

BR

Alice

 

0 Kudos
Reply

2,553 Views
_Ferrari_
Contributor V

Dear @Alice_Yang 

thank you for your email.

So it menas that it is impossible to share schematics of PLU between projects. My problem is that I have designed a schematic, and I want to import it in new project in which I have to modify it, without redraw it from scratch

0 Kudos
Reply

2,547 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @_Ferrari_ 

 

"So it menas that it is impossible to share schematics of PLU between projects. My problem is that I have designed a schematic, and I want to import it in new project in which I have to modify it,"

->> What about the projects meaning? Project under MCUXpresso IDE OR PLU tool? 

 

BR

Alice

0 Kudos
Reply