Content originally posted in LPCWare by acelink1 on Wed Feb 19 19:08:10 MST 2014
Hi Guys, I have a serious problem.
I have written a small Assembly program in a .S file. When I build the whole project Xpresso reads and builds the .S file. I know this because I deliberately wrote NOP #4 instead of NOP just to see if Expresso would error and it did. So I know Expresso is reading and building my Assembler .S file.
In the main.c file is just the basic default setup of the LPC4357 and a while loop at the end of the C program.
I have entered this line before the while loop to externally include my assembler program. Is this correct?
extern int assem_program;
Now when I build the whole project and view the disassembly my assembler program is not there only the while loop in C is there.
Why isn't Xpresso including my .S file when building.
Somebody please explain before I have no hair left :)
Oh, I don't know C++ I'm an assembler programmer.
Pete