Content originally posted in LPCWare by smachell on Wed Feb 19 14:28:43 MST 2014
Just ported a project from IAR to LPCXpresso. Saw notes that Segger J-Link is not supported and I should get a LPC-LINK2.
So my LPC-LINK2 just arrived - when I tried to debug it never downloaded new code like the notes seemed to indicate.
In the Debugger settings I tried LPC-LINK(WinUSB), LPC-LINK, and Redlink Server.
Redlink Server seems to be the one that sort of works (it never downloaded any firmware to LPC-LINK2).
What is more disturbing is the message I get: Redlink Server does not support NXP 2378
Bummer because my target has a an LPC2378.
Does that mean I'm screwed as far as the LPC-LINK2 goes.
Does it mean I have to buy a more expensive Redlink Red Probe+ or will that not work with LPC2378 ARM7 either?
Why can't you support J-Link. I have two of them in my office. Heck even Freescale Codewarrior works with them.