C with CMSIS or C++ Default generated projects - potential problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

C with CMSIS or C++ Default generated projects - potential problem

236件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by annodomini2 on Fri Jan 29 17:21:51 MST 2010
If I create a C++ (with or without CMSIS) or a C with CMSIS project for the LPC1343, they will not build straight away.

I have been through the Knowledge base and CMSIS documentation, am I missing something or should these work out of the box?
0 件の賞賛
2 返答(返信)

202件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Sat Jan 30 08:00:59 MST 2010
In addition to the pointer to a previous post from rkiryanov, if you are creating CMSIS based projects, the most likely thing that might go wrong is that your current project workspace does not contain the appropriate CMSIS library project (containing the CMSIS headers and library functions).

For more information on this see:

Section 6.5 of the LPCXpresso Getting started at:
http://ics.nxp.com/support/documents/microcontrollers/pdf/lpcxpresso.getting.started.pdf

"Support for CMSIS" knowledgebase entry at:
http://lpcxpresso.code-red-tech.com/LPCXpresso/node/21

If these don't get you up and running, then please post more details of exactly what the build error you see actually is.

Regards,

CodeRedSupport
0 件の賞賛

202件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rkiryanov on Sat Jan 30 03:24:53 MST 2010
http://knowledgebase.nxp.com/showthread.php?t=20
0 件の賞賛