Anybody want a little project?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Anybody want a little project?

280 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by OXO on Thu Feb 02 02:00:32 MST 2012
I have too much to do and I need a small project doing. It's an add-on to a much bigger proj.

I have a 1765 based module which has a USBMSD code, and works fine.

I need to add a HID device and make this into a composite USB device. I also need a small windows app which will talk to the HID and allow display and setting of parameters. The windows app will be a dialog app.

If you are in europe I can supply a board to run the code on, otherwise, maybe you could do it with a lpcxpresso board.

I will be paying for this work..

email me..
spiritsail at the hot mail dot com

Chris
0 Kudos
5 Replies

274 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by stalisman on Thu Feb 02 09:04:30 MST 2012
The composite part isn't too difficult.

The HID report definitions can be a pain due to the poor documentation but there are tools to aid in their development.

The Windows side is a different ball game altogether.  The two devices will enumerate sepparately which is fine. Your dialog application will however have to sign up to receive the reports from the new HID device and that will require a little in depth knowledge of how Windows works.

I'd suggest advertising on a Windows site also for the latter.
0 Kudos

274 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by OXO on Thu Feb 02 08:23:34 MST 2012
There is CAN, but I've already done that part :)
0 Kudos

274 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu Feb 02 06:29:10 MST 2012
Sorry, what I was trying to say is that there's unfortunately no CAN in your 'little project'  :)
0 Kudos

274 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by OXO on Thu Feb 02 06:11:58 MST 2012

Quote: Zero
Damned, no CAN inside :rolleyes:



Pardon?
0 Kudos

274 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu Feb 02 05:03:18 MST 2012
Damned, no CAN inside :rolleyes:
0 Kudos