What toolchains are compatible with LPC-Link ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What toolchains are compatible with LPC-Link ?

1,628 次查看
lpcware-support
Senior Contributor I

LPC-Link, the debug probe built into the original LPCXpresso board design, is only compatible with the LPCXpresso IDE (and the now discontinued Code Red Technologies Red Suite product).

If you want a debug probe suitable for use with another toolchain, such as Keil or IAR, then you should consider LPC-Link2 - either in standalone form or as built in to the LPCXpresso V2 boards.

标签 (1)
标记 (2)
0 项奖励
回复
0 回复数